<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: two  9S12 questions</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/two-9S12-questions/m-p/142004#M3377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello and Welcome,&lt;BR /&gt;&lt;BR /&gt;I don't think you will be able to find a pin to pin replacement.&lt;BR /&gt;If it exists, you should look at the MC9S12D64 or MC9S12DG128.&lt;BR /&gt;There is a D32, but it seems to be based on the MC9S12D64.&lt;BR /&gt;&lt;BR /&gt;For question 2, I would use the ADC module. &lt;BR /&gt;On some MCUs you have the possibility to wake up on comparison of a value.&lt;BR /&gt;&lt;BR /&gt;I hope this help,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Aug 2007 22:08:13 GMT</pubDate>
    <dc:creator>Alban</dc:creator>
    <dc:date>2007-08-02T22:08:13Z</dc:date>
    <item>
      <title>two  9S12 questions</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/two-9S12-questions/m-p/142003#M3376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;first question I have is&amp;nbsp; :&lt;/DIV&gt;&lt;DIV&gt;Is there a MCU that has the same pinout as the MC9S12DP512 but without the 512&amp;nbsp; perhaps 32k or 64k&amp;nbsp; the pinout has to be the same though.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Next question is on the software side.&amp;nbsp; Is there a comparitor on the 9S12 chips to invoke an interupt on the compared differences while reading from peripherals&amp;nbsp; such as&amp;nbsp; an analog acceleromter ?&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Dennis Momy&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2007 21:52:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/two-9S12-questions/m-p/142003#M3376</guid>
      <dc:creator>dmomy</dc:creator>
      <dc:date>2007-08-02T21:52:23Z</dc:date>
    </item>
    <item>
      <title>Re: two  9S12 questions</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/two-9S12-questions/m-p/142004#M3377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello and Welcome,&lt;BR /&gt;&lt;BR /&gt;I don't think you will be able to find a pin to pin replacement.&lt;BR /&gt;If it exists, you should look at the MC9S12D64 or MC9S12DG128.&lt;BR /&gt;There is a D32, but it seems to be based on the MC9S12D64.&lt;BR /&gt;&lt;BR /&gt;For question 2, I would use the ADC module. &lt;BR /&gt;On some MCUs you have the possibility to wake up on comparison of a value.&lt;BR /&gt;&lt;BR /&gt;I hope this help,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2007 22:08:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/two-9S12-questions/m-p/142004#M3377</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-08-02T22:08:13Z</dc:date>
    </item>
    <item>
      <title>Re: two  9S12 questions</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/two-9S12-questions/m-p/142005#M3378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;The S12Dx was designed as a family with flash sizes 32, 64, 128, 256, and 512. Check with your supplier to see the availability of these.&lt;/DIV&gt;&lt;DIV&gt;In terms of pinout it depends what you mean. The general pinout is the same across the family but the smaller the flash size then the fewer the on-chip peripherals as well so for example the 64k part does not have 5 CAN modules.&lt;/DIV&gt;&lt;DIV&gt;Decide which peripherals you need for your application then check the availability of these on the selector guides.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2007 16:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/two-9S12-questions/m-p/142005#M3378</guid>
      <dc:creator>Steve</dc:creator>
      <dc:date>2007-08-03T16:38:08Z</dc:date>
    </item>
    <item>
      <title>Re: two  9S12 questions</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/two-9S12-questions/m-p/142006#M3379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Speaking about selection guides, could you shed some light on what happened to non-automotive SG1006.pdf? I can't find recent version of it, only Q1.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2007 16:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/two-9S12-questions/m-p/142006#M3379</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2007-08-03T16:57:06Z</dc:date>
    </item>
  </channel>
</rss>