<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic communication problem in debugging M68EVB9S12C32 in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/communication-problem-in-debugging-M68EVB9S12C32/m-p/140857#M3150</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I just start to use the M68EVB9S12C32 evaluation board from Axiom, yet&amp;nbsp;got stuck at the very beginning. Following the manual of this evaluation board, I built a empty test project&amp;nbsp;via&amp;nbsp;the wizard of CodeWarrior for HC12 (4.5). After connecting the SCI port with COM1 using the provided cable, and power on the target board, I tried to enter&amp;nbsp;debug, but after the progress bar displays "erased flash",..., "executing&amp;nbsp;xxx.cmd&amp;nbsp;", a connection error appears showing "the target does not respond to communication request", and&amp;nbsp;the progress bar is located behind this message area; please refer to the attached screenshot of this error message. If&amp;nbsp; the&amp;nbsp; EVB board is powered off, and do the debug again, the same error message appears but&amp;nbsp;the progress bar doesn't.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I then tried the companion HCS Serial Monitor Interface(a Visual Basic soft),&amp;nbsp;the target board can be initialized successfully, and response is also received from the target!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Anybody can give&amp;nbsp;suggestions?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What follows are some details of the settings.&lt;/DIV&gt;&lt;DIV&gt;The project is set&amp;nbsp;to serial monitor mode, and main.c file contains only the following two lines:&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;EnableInterrupts;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;for( ; ; ) {}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;The jumpers are set as follows:&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-CTS_EN -&amp;gt; open&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-RTS_EN -&amp;gt; open&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-RX_EN -&amp;gt; close&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-ROM_EN -&amp;gt; GND&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-MODC -&amp;gt; +5V&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-MODB -&amp;gt; GND&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-MODA -&amp;gt; GND&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-OSC_SEL2 -&amp;gt; EXTERNAL&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-OSC_SEL1 -&amp;gt; EXT_CLOCK&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-SW1_EN -&amp;gt; closed&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-LED_EN -&amp;gt; close&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-CAN_RXEN -&amp;gt; open&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-CAN_TXEN -&amp;gt; open&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;SW7 switch&amp;nbsp;-&amp;gt; OFF&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;Different baud rates are tried,&amp;nbsp;like 115200, 9600, 192000, etc., but without effect.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;I also tested under the original CodeWarrior 3.0 and installed the service pack, the debugger hangs for a long time then gives HI-WAVE error "target not ready or not connected on COM1".&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;P&gt;Message Edited by roboy on &lt;SPAN class="date_text"&gt;2006-12-21&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;09:28 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Message Edited by roboy on &lt;SPAN class="date_text"&gt;2006-12-21&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;09:41 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Dec 2006 17:26:35 GMT</pubDate>
    <dc:creator>roboy</dc:creator>
    <dc:date>2006-12-21T17:26:35Z</dc:date>
    <item>
      <title>communication problem in debugging M68EVB9S12C32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/communication-problem-in-debugging-M68EVB9S12C32/m-p/140857#M3150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I just start to use the M68EVB9S12C32 evaluation board from Axiom, yet&amp;nbsp;got stuck at the very beginning. Following the manual of this evaluation board, I built a empty test project&amp;nbsp;via&amp;nbsp;the wizard of CodeWarrior for HC12 (4.5). After connecting the SCI port with COM1 using the provided cable, and power on the target board, I tried to enter&amp;nbsp;debug, but after the progress bar displays "erased flash",..., "executing&amp;nbsp;xxx.cmd&amp;nbsp;", a connection error appears showing "the target does not respond to communication request", and&amp;nbsp;the progress bar is located behind this message area; please refer to the attached screenshot of this error message. If&amp;nbsp; the&amp;nbsp; EVB board is powered off, and do the debug again, the same error message appears but&amp;nbsp;the progress bar doesn't.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I then tried the companion HCS Serial Monitor Interface(a Visual Basic soft),&amp;nbsp;the target board can be initialized successfully, and response is also received from the target!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Anybody can give&amp;nbsp;suggestions?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What follows are some details of the settings.&lt;/DIV&gt;&lt;DIV&gt;The project is set&amp;nbsp;to serial monitor mode, and main.c file contains only the following two lines:&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;EnableInterrupts;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;for( ; ; ) {}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;The jumpers are set as follows:&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-CTS_EN -&amp;gt; open&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-RTS_EN -&amp;gt; open&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-RX_EN -&amp;gt; close&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-ROM_EN -&amp;gt; GND&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-MODC -&amp;gt; +5V&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-MODB -&amp;gt; GND&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-MODA -&amp;gt; GND&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-OSC_SEL2 -&amp;gt; EXTERNAL&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-OSC_SEL1 -&amp;gt; EXT_CLOCK&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-SW1_EN -&amp;gt; closed&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-LED_EN -&amp;gt; close&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-CAN_RXEN -&amp;gt; open&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;-CAN_TXEN -&amp;gt; open&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;gt;SW7 switch&amp;nbsp;-&amp;gt; OFF&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;Different baud rates are tried,&amp;nbsp;like 115200, 9600, 192000, etc., but without effect.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 2;"&gt;I also tested under the original CodeWarrior 3.0 and installed the service pack, the debugger hangs for a long time then gives HI-WAVE error "target not ready or not connected on COM1".&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;P&gt;Message Edited by roboy on &lt;SPAN class="date_text"&gt;2006-12-21&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;09:28 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Message Edited by roboy on &lt;SPAN class="date_text"&gt;2006-12-21&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;09:41 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Dec 2006 17:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/communication-problem-in-debugging-M68EVB9S12C32/m-p/140857#M3150</guid>
      <dc:creator>roboy</dc:creator>
      <dc:date>2006-12-21T17:26:35Z</dc:date>
    </item>
    <item>
      <title>Re: communication problem in debugging M68EVB9S12C32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/communication-problem-in-debugging-M68EVB9S12C32/m-p/140858#M3151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Royboy,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This question may be best answered by Freescale's technical support group. You can submit a service request through the following website: &lt;A href="https://www.freescale.com/webapp/ruhp.login.framework" rel="nofollow" target="_blank"&gt;https://www.freescale.com/webapp/ruhp.login.framework&lt;/A&gt;&amp;nbsp;or you can email them at &lt;A href="mailto:support@freescale.com" rel="nofollow" target="_blank"&gt;support@freescale.com&lt;/A&gt;&amp;nbsp; Make sure to provide them with as much details as possible so that they can respond to your questions properly.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Nina&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2007 04:41:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/communication-problem-in-debugging-M68EVB9S12C32/m-p/140858#M3151</guid>
      <dc:creator>NLFSJ</dc:creator>
      <dc:date>2007-01-09T04:41:32Z</dc:date>
    </item>
    <item>
      <title>Re: communication problem in debugging M68EVB9S12C32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/communication-problem-in-debugging-M68EVB9S12C32/m-p/140859#M3152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Problem solved.&lt;/DIV&gt;&lt;DIV&gt;I got a P&amp;amp;E usb Multilink pod, and reflashed the AN2548 serial monitor, then everything turns ok.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2007 17:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/communication-problem-in-debugging-M68EVB9S12C32/m-p/140859#M3152</guid>
      <dc:creator>roboy</dc:creator>
      <dc:date>2007-01-12T17:24:31Z</dc:date>
    </item>
  </channel>
</rss>