<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: FlexCAN</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexCAN/m-p/140338#M3090</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;volatile word* data_base = &amp;amp;FCMB0_DATA0;volatile word* control_base = &amp;amp;FCMB0_Control;volatile word* data_reg;volatile word* control_reg;#define reg_offs 0x8...void Readbuff(byte numbuf, byte* data){   byte i, RxCode, length;      data_reg = data_base + numbuf*reg_offs;   control_reg = control_base + numbuf*reg_offs;         RxCode = (*control_reg &amp;amp; 0xF0)&amp;gt;&amp;gt;4;  /* read RxCode */     *control_reg = (*control_reg &amp;amp; 0xFF0F); /* hold inactive Rx buffer */   length = (byte)(*control_reg &amp;amp; 0x0F); /* length of the received message */   for (i=0; i&amp;lt;length/2; i++)   {      *data++ = (byte)(*data_reg &amp;gt;&amp;gt; 8);      *data++ = (byte)(*data_reg);   }   if (length &amp;amp; 1)   *data = (byte)(*data_reg);  *control_reg = 0x40; /* set the message buffer code = Empty*/}....// CAN Tx-Rx interrupt function#pragma interrupt alignsp saveallvoid CANInterrupt(void){   byte rxBuff[8];      word BufFlags = getReg(FCIFLAG1);   setReg(FCIFLAG1,BufFlags);  /* clear interrupt flags */   if ((BufFlags &amp;amp; 0x02) &amp;gt; 0)  /* MB1 transmit */   {//  after transmition action code here   }   if ((BufFlags &amp;amp; 0x01) &amp;gt; 0)  /* MB0 receive */   {      Readbuff(0,rxBuff);//  another receive action code here   }}&lt;/PRE&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Try this code. This is simple example of read of the received DATA frame from CAN buffer 0.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Message Edited by Alexey on &lt;SPAN class="date_text"&gt;2006-12-23&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;12:32 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Oct 2020 08:40:34 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2020-10-29T08:40:34Z</dc:date>
    <item>
      <title>FlexCAN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexCAN/m-p/140337#M3089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I am a newbie with the flexCAN. I have two 56f8300DEMO boards and I want experiment connect them with CAN. I've not freescaleCAN bean licensed so I need for a very simple example code for tx and rx tasks. I tried to develop my own code, but only tx work, no rx.&lt;BR /&gt;&lt;BR /&gt;I appreciate some help to me.&lt;BR /&gt;&lt;BR /&gt;thanks in advance&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Dec 2006 00:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexCAN/m-p/140337#M3089</guid>
      <dc:creator>Nerone</dc:creator>
      <dc:date>2006-12-17T00:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexCAN/m-p/140338#M3090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;volatile word* data_base = &amp;amp;FCMB0_DATA0;volatile word* control_base = &amp;amp;FCMB0_Control;volatile word* data_reg;volatile word* control_reg;#define reg_offs 0x8...void Readbuff(byte numbuf, byte* data){   byte i, RxCode, length;      data_reg = data_base + numbuf*reg_offs;   control_reg = control_base + numbuf*reg_offs;         RxCode = (*control_reg &amp;amp; 0xF0)&amp;gt;&amp;gt;4;  /* read RxCode */     *control_reg = (*control_reg &amp;amp; 0xFF0F); /* hold inactive Rx buffer */   length = (byte)(*control_reg &amp;amp; 0x0F); /* length of the received message */   for (i=0; i&amp;lt;length/2; i++)   {      *data++ = (byte)(*data_reg &amp;gt;&amp;gt; 8);      *data++ = (byte)(*data_reg);   }   if (length &amp;amp; 1)   *data = (byte)(*data_reg);  *control_reg = 0x40; /* set the message buffer code = Empty*/}....// CAN Tx-Rx interrupt function#pragma interrupt alignsp saveallvoid CANInterrupt(void){   byte rxBuff[8];      word BufFlags = getReg(FCIFLAG1);   setReg(FCIFLAG1,BufFlags);  /* clear interrupt flags */   if ((BufFlags &amp;amp; 0x02) &amp;gt; 0)  /* MB1 transmit */   {//  after transmition action code here   }   if ((BufFlags &amp;amp; 0x01) &amp;gt; 0)  /* MB0 receive */   {      Readbuff(0,rxBuff);//  another receive action code here   }}&lt;/PRE&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Try this code. This is simple example of read of the received DATA frame from CAN buffer 0.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Message Edited by Alexey on &lt;SPAN class="date_text"&gt;2006-12-23&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;12:32 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 08:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexCAN/m-p/140338#M3090</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2020-10-29T08:40:34Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexCAN/m-p/140339#M3091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks you!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Dec 2006 00:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/FlexCAN/m-p/140339#M3091</guid>
      <dc:creator>Nerone</dc:creator>
      <dc:date>2006-12-24T00:08:24Z</dc:date>
    </item>
  </channel>
</rss>