<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Flash programming</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-programming/m-p/140317#M3082</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;AFAIK, If there are no errata stopping it, then the bootloader can have full rain on the Flash within secure mode. In fact, if it were not able to erase Flash, then the MCU could not be unsecured so it is in the design.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Jun 2006 20:38:18 GMT</pubDate>
    <dc:creator>imajeff</dc:creator>
    <dc:date>2006-06-20T20:38:18Z</dc:date>
    <item>
      <title>Flash programming</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-programming/m-p/140316#M3081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi..&lt;/DIV&gt;&lt;DIV&gt;When the micro is in the secure state, Can I program the flash memory from within the bootloader?&lt;/DIV&gt;&lt;DIV&gt;Or the&amp;nbsp;bootloader must leave the micro in unsecured state?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2006 19:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-programming/m-p/140316#M3081</guid>
      <dc:creator>marchè</dc:creator>
      <dc:date>2006-06-20T19:51:31Z</dc:date>
    </item>
    <item>
      <title>Re: Flash programming</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-programming/m-p/140317#M3082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;AFAIK, If there are no errata stopping it, then the bootloader can have full rain on the Flash within secure mode. In fact, if it were not able to erase Flash, then the MCU could not be unsecured so it is in the design.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2006 20:38:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-programming/m-p/140317#M3082</guid>
      <dc:creator>imajeff</dc:creator>
      <dc:date>2006-06-20T20:38:18Z</dc:date>
    </item>
    <item>
      <title>Re: Flash programming</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-programming/m-p/140318#M3083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;There is an errata stopping it for the old "B" masks:&lt;BR /&gt;&lt;BR /&gt;In normal single chip mode, when security is enabled, it is not possible to launch the Program ($20), Sector-Erase ($40) and Erase- Verify ($05) commands in the Flash. The Mass-Erase ($41) command can be launched.&lt;BR /&gt;&lt;BR /&gt;Same goes for EEPROM.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2006 17:57:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-programming/m-p/140318#M3083</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2006-06-26T17:57:03Z</dc:date>
    </item>
    <item>
      <title>Re: Flash programming</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-programming/m-p/140319#M3084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;With the 9S12C32 in secure mode it is possible to erase and program FLASH. I added things to the SErial mon for this purpose.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2006 02:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flash-programming/m-p/140319#M3084</guid>
      <dc:creator>Ilocano</dc:creator>
      <dc:date>2006-07-05T02:12:51Z</dc:date>
    </item>
  </channel>
</rss>