<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Flexray</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139967#M2984</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;There is a common error I have seen with these boards I have never used.&lt;BR /&gt;When you look in the debugger where you should see the memory of the daughter board (FRDC) you see an echo of the address as values.&lt;BR /&gt;&lt;BR /&gt;The reason is that the S12X has not been enabled for expanded mode.&lt;BR /&gt;&lt;BR /&gt;Check if external signals are set-up properly.&lt;BR /&gt;&lt;BR /&gt;Flexray is quite new and reserved for Automotive under license (for now).&lt;BR /&gt;Thereofre I doubt many people here don't even know what it is about.&lt;BR /&gt;A Service Request seems the more efficient way for you.&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Dec 2006 18:25:44 GMT</pubDate>
    <dc:creator>Alban</dc:creator>
    <dc:date>2006-12-14T18:25:44Z</dc:date>
    <item>
      <title>Flexray</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139966#M2983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;We have purchased several SK-S12XDP512-A evaluation boards&lt;BR /&gt;and several Freescale Generic FlexRay Daughter Cards&lt;BR /&gt;(FRDC) FLXRAYIPMFR4300.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The provided Flexray demo code does not work: when the demo&lt;/DIV&gt;&lt;DIV&gt;code is running, both flexray line remains high&lt;BR /&gt;and do not change. Also, for instance if&amp;nbsp;I try to read MVR&lt;BR /&gt;register from MFR4300, the returned value is not 0x3535 (version number).&lt;/DIV&gt;&lt;DIV&gt;Please let&amp;nbsp;me know how we can run the demo code on&lt;BR /&gt;SK-S12XDP512-A evaluation board and (FRDC) FLXRAYIPMFR4300,&lt;BR /&gt;what needs to be checked or added to the demo code.&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;Thanks,&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Dec 2006 04:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139966#M2983</guid>
      <dc:creator>AKorn</dc:creator>
      <dc:date>2006-12-14T04:21:07Z</dc:date>
    </item>
    <item>
      <title>Re: Flexray</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139967#M2984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;There is a common error I have seen with these boards I have never used.&lt;BR /&gt;When you look in the debugger where you should see the memory of the daughter board (FRDC) you see an echo of the address as values.&lt;BR /&gt;&lt;BR /&gt;The reason is that the S12X has not been enabled for expanded mode.&lt;BR /&gt;&lt;BR /&gt;Check if external signals are set-up properly.&lt;BR /&gt;&lt;BR /&gt;Flexray is quite new and reserved for Automotive under license (for now).&lt;BR /&gt;Thereofre I doubt many people here don't even know what it is about.&lt;BR /&gt;A Service Request seems the more efficient way for you.&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Dec 2006 18:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139967#M2984</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2006-12-14T18:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: Flexray</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139968#M2985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Alban,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for the reply.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Could you please help me out with the steps that are needed to&lt;BR /&gt;run flexray demo code on SK-S12XDP512-A and (FRDC) FLXRAYIPMFR4300?&lt;/DIV&gt;&lt;DIV&gt;I guess this would be also helpful for all people who deal with flexray boards.&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;Please correct my list of steps:&lt;/DIV&gt;&lt;DIV&gt;1. Attach each FRDC to its SK-S12XDP512-A.&lt;/DIV&gt;&lt;DIV&gt;2. Connect flexray channel connector FR1 on the first FRDC&lt;BR /&gt;to the other FR1 on the other FRDC using two wires.&lt;/DIV&gt;&lt;DIV&gt;3. FDRC Jumpers: all jumpers are on except:&lt;BR /&gt;JG1 set to +5V,&lt;BR /&gt;JG14 and JG15 set to connect pins 1 and 2&lt;/DIV&gt;&lt;DIV&gt;4. FDRC DIP switches:&lt;/DIV&gt;&lt;DIV&gt;SW1: Need to activate Hardware Reset&lt;BR /&gt;1 - off // Ext. reset&lt;BR /&gt;2 - off // Ext. reset. This duplictaes the switch 1???&lt;BR /&gt;3 - ON&amp;nbsp; // Hardware reset&lt;BR /&gt;4 - off // Manual reset&lt;/DIV&gt;&lt;DIV&gt;SW2: Need to select S12 synchronous memory interface:&lt;BR /&gt;1 - off // IF_SEL1 high is off&lt;BR /&gt;2 - ON // IF_SEL1 low is on,&amp;nbsp; IF_SEL1=LOW&lt;BR /&gt;3 - off // CHICLK_CC high is off&amp;nbsp;&lt;BR /&gt;4 - ON // CHICLK_CC low is on, dont care about CHICLK_CC&lt;BR /&gt;5 - ON // IF_SEL0 high is on&lt;BR /&gt;6 - off // IF_SEL0 low is off,&amp;nbsp; IF_SEL1=HIGH&lt;BR /&gt;7 - off // Unconncted&lt;BR /&gt;8 - off // dont care about CHICLK_EN&lt;/DIV&gt;&lt;DIV&gt;SW3: We don't need to set up clock output, so don't care about these&lt;BR /&gt;1 - off // DBG2/CLK_S0 high is off&lt;BR /&gt;2 - ON // DBG2/CLK_S0 low is on&lt;BR /&gt;3 - off // BSEL1#/DBG0/CLK_S1 high is off&amp;nbsp;&lt;BR /&gt;4 - ON // BSEL1#/DBG0/CLK_S1 low is on&amp;nbsp;&lt;BR /&gt;5 - off // BSEL0#/DBG1/CLK_S0 high is off&amp;nbsp;&lt;BR /&gt;6 - ON&amp;nbsp; // BSEL0#/DBG1/CLK_S0 low is on&amp;nbsp;&lt;BR /&gt;7 - off // DBG3/CLK_S1/BGE2 high is off&lt;BR /&gt;8 - ON&amp;nbsp; // DBG3/CLK_S1/BGE2 high is on&lt;/DIV&gt;&lt;DIV&gt;5. Install CodeWarrior&lt;BR /&gt;6. Install CW Components v4.5&lt;BR /&gt;7. Complile and program the available demo project&lt;BR /&gt;cfg1_node1.mcp for the first boards.&lt;BR /&gt;8. Complile and program the available demo project&lt;BR /&gt;cfg1_node2.mcp for the second boards.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I guess at this point we should be to detect flexray messages&lt;BR /&gt;in the static segment by using a scope on the FR connectors.&lt;/DIV&gt;&lt;DIV&gt;I saw just both lines on FR connector were high.&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;When I modified the code in order to read a version register MVR,&lt;BR /&gt;the returned value was 0x1F1F instead of 0x3535.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thank you,&lt;/DIV&gt;&lt;DIV&gt;Alex&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Dec 2006 00:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139968#M2985</guid>
      <dc:creator>AKorn</dc:creator>
      <dc:date>2006-12-15T00:12:51Z</dc:date>
    </item>
    <item>
      <title>Re: Flexray - SK-S12XDP512-A and (FRDC) FLXRAYIPMFR4300</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139969#M2986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Alex,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm sorry but I don't have the slightest clue.&lt;/DIV&gt;&lt;DIV&gt;I only touched them a couple of times and don't have any board now.&lt;/DIV&gt;&lt;DIV&gt;The status of jumpers should be reported in the PDF of the MFR4300 FRDC.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The other things that is coming back to my mind is that&amp;nbsp;a FRDC connector on the first SofTec boards (same ref you have) was put the wrong way round. But it should have been obvious if you couldn't plug the daughter board.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Alban.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Dec 2006 00:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139969#M2986</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2006-12-15T00:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: Flexray - SK-S12XDP512-A and (FRDC) FLXRAYIPMFR4300</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139970#M2987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Akorn&lt;BR /&gt;&lt;BR /&gt;*Did you get ahead with the project/ fix the MNR problem ?&lt;BR /&gt;&lt;BR /&gt;*In addition to the steps you have listed, you need to connect the GROUNDS of both boards.&lt;BR /&gt;&lt;BR /&gt;When I tried to use a MFR4200 with a S12X eval board that you have, I couldn't read the MNR as expected&lt;BR /&gt;&lt;BR /&gt;The signals (Addr, data and chip select)on the S12X side look correct to me.&lt;BR /&gt;I have sent the FRDC board for replacement (with a 4300 FRDC) as I had some other h/w problems with it.&lt;BR /&gt;&lt;BR /&gt;Have you had a chance to use the S12X JTAG debugger ?&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Vi&lt;P&gt;Message Edited by _Alien_ on &lt;SPAN class="date_text"&gt;2007-02-01&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;10:46 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2007 06:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Flexray/m-p/139970#M2987</guid>
      <dc:creator>vikram_iyengar</dc:creator>
      <dc:date>2007-02-02T06:37:16Z</dc:date>
    </item>
  </channel>
</rss>