<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Strange behavior of WinIDEA in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-behavior-of-WinIDEA/m-p/139409#M2888</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I load a program in the flash of a MC9S12E128 and then i debug "step by step" (F11) and the program works fine. But if i click on the "run" button (or F5) the flash seems to be erased (FFFF all over it). Even if i set a breakpoint just the line below the line i hit the F5, i don't reach the breakpoint.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What can it be ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2006 18:15:58 GMT</pubDate>
    <dc:creator>Gizzzmo</dc:creator>
    <dc:date>2006-06-13T18:15:58Z</dc:date>
    <item>
      <title>Strange behavior of WinIDEA</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-behavior-of-WinIDEA/m-p/139409#M2888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I load a program in the flash of a MC9S12E128 and then i debug "step by step" (F11) and the program works fine. But if i click on the "run" button (or F5) the flash seems to be erased (FFFF all over it). Even if i set a breakpoint just the line below the line i hit the F5, i don't reach the breakpoint.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What can it be ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2006 18:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-behavior-of-WinIDEA/m-p/139409#M2888</guid>
      <dc:creator>Gizzzmo</dc:creator>
      <dc:date>2006-06-13T18:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: Strange behavior of WinIDEA</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-behavior-of-WinIDEA/m-p/139410#M2889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;this can be because of a wrong settings of winIdea.&lt;BR /&gt;Please check the clock and PLL settings.&lt;BR /&gt;Showing all memory locations as 0xFF is mostly the result of a wrong clock setting.&lt;BR /&gt;Also check if code with the breakpoint is reachable. If not winIdea would never stop.&lt;BR /&gt;If ths does not help refer to the knowledge base (http://www.isystem.com/technical/FAQ/).&lt;BR /&gt;&lt;BR /&gt;Hope this helps&lt;BR /&gt;Regards,&lt;BR /&gt;Christian&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2006 01:43:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Strange-behavior-of-WinIDEA/m-p/139410#M2889</guid>
      <dc:creator>christian</dc:creator>
      <dc:date>2006-06-14T01:43:10Z</dc:date>
    </item>
  </channel>
</rss>