<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Erase of Flash Causes Lock  up in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Erase-of-Flash-Causes-Lock-up/m-p/137830#M2660</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Has anyone caused a device to lockup by trying&amp;nbsp; too erase flash locations and if so is there a way of being able to connect to the device again?&amp;nbsp; I am trying&amp;nbsp; to implement a bootloader and&amp;nbsp;issued a Erase_Flash_Sector command passing it the address 0xEF00 and the device locked up such&amp;nbsp; that I am no loonger able to connect to it with the P&amp;amp;E Multilink.&amp;nbsp; Is there a way to fix this or doo I have to replace the device?&amp;nbsp; What did I do wrong?&lt;/DIV&gt;&lt;DIV&gt;Many thanks&lt;/DIV&gt;&lt;DIV&gt;Morag&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Nov 2006 23:54:28 GMT</pubDate>
    <dc:creator>morag</dc:creator>
    <dc:date>2006-11-23T23:54:28Z</dc:date>
    <item>
      <title>Erase of Flash Causes Lock  up</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Erase-of-Flash-Causes-Lock-up/m-p/137830#M2660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Has anyone caused a device to lockup by trying&amp;nbsp; too erase flash locations and if so is there a way of being able to connect to the device again?&amp;nbsp; I am trying&amp;nbsp; to implement a bootloader and&amp;nbsp;issued a Erase_Flash_Sector command passing it the address 0xEF00 and the device locked up such&amp;nbsp; that I am no loonger able to connect to it with the P&amp;amp;E Multilink.&amp;nbsp; Is there a way to fix this or doo I have to replace the device?&amp;nbsp; What did I do wrong?&lt;/DIV&gt;&lt;DIV&gt;Many thanks&lt;/DIV&gt;&lt;DIV&gt;Morag&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 23:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Erase-of-Flash-Causes-Lock-up/m-p/137830#M2660</guid>
      <dc:creator>morag</dc:creator>
      <dc:date>2006-11-23T23:54:28Z</dc:date>
    </item>
    <item>
      <title>Re: Erase of Flash Causes Lock  up</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Erase-of-Flash-Causes-Lock-up/m-p/137831#M2661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You have likely cleared the address 0x7FFF0F and in doing so caused the MCU’s Flash Security to become enabled. If this byte is anything other than 0xFE the device cannot be accessed by debugger, this is to prevent unauthorised access to the contents of flash. There are two ways to unsecure the flash: using Back Door Access or by performing a mass erase. The latter requires an 8byte password to be set before the device is secured and since this is unlikely in this case, the only option is to mass erase the flash.&lt;BR /&gt;&lt;BR /&gt;To do so you should use the enable the recovery command “unlock_flash_on_connect 1” in CodeWarrior in the memory configuration (.cfg) file.&lt;BR /&gt;&lt;BR /&gt;More info can be found on page 100 of the Data Sheet:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.freescale.com/files/dsp/doc/data_sheet/MC56F8323.pdf" rel="nofollow" target="_blank"&gt;Link&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Danny&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Nov 2006 00:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Erase-of-Flash-Causes-Lock-up/m-p/137831#M2661</guid>
      <dc:creator>DannyM83</dc:creator>
      <dc:date>2006-11-24T00:29:46Z</dc:date>
    </item>
    <item>
      <title>Re: Erase of Flash Causes Lock  up</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Erase-of-Flash-Causes-Lock-up/m-p/137832#M2662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the same problem with 84789 microcontroller.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did not erase the address&amp;nbsp;&lt;SPAN&gt;0x7FFF0F&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;i used the following command:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;hfm_command(FTFL_ERASE_SECTOR, (UInt16*)(i*FLASHP_PAGE_SIZE + PFLASH_START_ADDR), 0, 0);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;where&amp;nbsp;&lt;SPAN&gt;PFLASH_START_ADDR &amp;nbsp;is 0x3000.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;After it, i think the chip is locked. I cannot program it any more to try fix the problem.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;I dont want to replace chip.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;I am using MCU 10.2 (new code warrior for microcontrollers MCU56F84789 (32 bit) with USB TAP.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 14px;"&gt;Please tell what should i do to first remove the unclock and then what code i should run in order to be able to write&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 14px;"&gt;and clear the memory for boot loader procedure.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 14px;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 14px;"&gt;Eli&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2012 15:16:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Erase-of-Flash-Causes-Lock-up/m-p/137832#M2662</guid>
      <dc:creator>EliArad</dc:creator>
      <dc:date>2012-06-20T15:16:12Z</dc:date>
    </item>
  </channel>
</rss>