<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Softec HCS12 Starter Kit in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Softec-HCS12-Starter-Kit/m-p/136255#M2377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Found the problem. Compared the Debugger files named SofTec,ini&lt;BR /&gt;&lt;BR /&gt;They were different, so I replaced the nonworking one with the working example.&lt;BR /&gt;&lt;BR /&gt;I posted a detailed explanation on the Softec forum:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.softecmicro.com/forum/showthread.php?s=&amp;amp;postid=1471#post1471" target="test_blank"&gt;http://www.softecmicro.com/forum/showthread.php?s=&amp;amp;postid=1471#post1471&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Nov 2006 00:57:22 GMT</pubDate>
    <dc:creator>JohnnyP</dc:creator>
    <dc:date>2006-11-13T00:57:22Z</dc:date>
    <item>
      <title>Softec HCS12 Starter Kit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Softec-HCS12-Starter-Kit/m-p/136254#M2376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Anyone else using the Softec PK-HCS12C32 Starter Kit? I can't get it to accept a test program written in assembly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I opened a new project in CodeWarrior and used the wizard to create an assembly project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The main.asm file has enough "stationery" code that it should execute as is, so I compiled it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Click debug in simultor mode, and the simulator runs it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Change to Softec target mode, then connect the kit to the pc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Click debug, True-Time simulator says communication error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Close True-time, open CodeWarrior, open Softec example ADC.mcp. This is a short C program that reads a pot, then outputs that value to LEDs connected to PTB&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Compile, click debug, Softec example loads and executes on started kit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;????&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for any help.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Nov 2006 14:52:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Softec-HCS12-Starter-Kit/m-p/136254#M2376</guid>
      <dc:creator>JohnnyP</dc:creator>
      <dc:date>2006-11-11T14:52:14Z</dc:date>
    </item>
    <item>
      <title>Re: Softec HCS12 Starter Kit</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Softec-HCS12-Starter-Kit/m-p/136255#M2377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Found the problem. Compared the Debugger files named SofTec,ini&lt;BR /&gt;&lt;BR /&gt;They were different, so I replaced the nonworking one with the working example.&lt;BR /&gt;&lt;BR /&gt;I posted a detailed explanation on the Softec forum:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.softecmicro.com/forum/showthread.php?s=&amp;amp;postid=1471#post1471" target="test_blank"&gt;http://www.softecmicro.com/forum/showthread.php?s=&amp;amp;postid=1471#post1471&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Nov 2006 00:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Softec-HCS12-Starter-Kit/m-p/136255#M2377</guid>
      <dc:creator>JohnnyP</dc:creator>
      <dc:date>2006-11-13T00:57:22Z</dc:date>
    </item>
  </channel>
</rss>