<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: Stand-alone BDM flash programmer for HCS12 ?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Stand-alone-BDM-flash-programmer-for-HCS12/m-p/135981#M2338</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've only thought about it. Hope you share with the rest of us when you get it going, since you believe in sharing &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;BR /&gt;&lt;BR /&gt;I think the UF32 would be great for it. I also don't see why you would need two memory cards. Mine would just be one, even If I do need to copy a special file on each one that is loaded into ram for the program.&lt;BR /&gt;&lt;BR /&gt;I think it would be an exellent solution for most small business, if develloped right and open-source.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 May 2006 20:54:33 GMT</pubDate>
    <dc:creator>imajeff</dc:creator>
    <dc:date>2006-05-16T20:54:33Z</dc:date>
    <item>
      <title>Stand-alone BDM flash programmer for HCS12 ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Stand-alone-BDM-flash-programmer-for-HCS12/m-p/135980#M2337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I wish to build a stand-alone Flash programmer using BDM for to program the HCS12 family using a flash card (1GB) for the program code and another flash card for to program a test program in RAM.&lt;/DIV&gt;&lt;DIV&gt;Does anyone has already&amp;nbsp;built something similar and can share&amp;nbsp;all the schematics, program code etc. maybe using a 9S12UF32 because it has the memory card interface ?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I know that there is a CyclonePro from P&amp;amp;E but it is not exactly what I am looking for.&lt;/DIV&gt;&lt;DIV&gt;Thanks a lot&lt;/DIV&gt;&lt;DIV&gt;cant66&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 May 2006 00:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Stand-alone-BDM-flash-programmer-for-HCS12/m-p/135980#M2337</guid>
      <dc:creator>cant</dc:creator>
      <dc:date>2006-05-14T00:12:25Z</dc:date>
    </item>
    <item>
      <title>Re: Stand-alone BDM flash programmer for HCS12 ?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Stand-alone-BDM-flash-programmer-for-HCS12/m-p/135981#M2338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've only thought about it. Hope you share with the rest of us when you get it going, since you believe in sharing &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;BR /&gt;&lt;BR /&gt;I think the UF32 would be great for it. I also don't see why you would need two memory cards. Mine would just be one, even If I do need to copy a special file on each one that is loaded into ram for the program.&lt;BR /&gt;&lt;BR /&gt;I think it would be an exellent solution for most small business, if develloped right and open-source.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2006 20:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Stand-alone-BDM-flash-programmer-for-HCS12/m-p/135981#M2338</guid>
      <dc:creator>imajeff</dc:creator>
      <dc:date>2006-05-16T20:54:33Z</dc:date>
    </item>
  </channel>
</rss>