<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HC12 IIC - Need help in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HC12-IIC-Need-help/m-p/124917#M219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I need some pointers/help in using IIC bus.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm using it to send data to a serial DAC (Max521), which is compatible with IIC. However, when I run my code I'm not convinced that&amp;nbsp;it is outputting the correct wave forms...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The code is something like this:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;for(;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif"&gt;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/A&gt; {&lt;BR /&gt;&amp;nbsp;init_IIC();&lt;BR /&gt;&amp;nbsp;write_IIC();&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;}&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;void init_IIC(){&lt;BR /&gt;&amp;nbsp;//Try Setting DDRJ&lt;BR /&gt;&amp;nbsp;DDRJ_DDRJ6=1;&lt;BR /&gt;&amp;nbsp;DDRJ_DDRJ7=1;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;IBFD = 0x20;&amp;nbsp; //Frequency divider&lt;BR /&gt;&amp;nbsp;IBAD = 0x1F;&amp;nbsp; //This is to set the slave address of the IIC&amp;nbsp; -- Doesn't really matter&amp;nbsp;?&lt;BR /&gt;&amp;nbsp;IBCR= 0xB0; //Enables, makes master, sets to transmit&lt;BR /&gt;&amp;nbsp;&amp;nbsp;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;void write_IIC() {&lt;BR /&gt;&amp;nbsp;IBDR = 0x50; // Slave Address 0101 0000&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;while(IBSR_TCF ==0 ) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;asm(nop);&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;IBDR= 0x00; //DAC0&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;while(IBSR_TCF ==0 ) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;asm(nop);&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;IBDR = 0xFF;//Activate DAC full tilt&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;while(IBSR_TCF ==0 ) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;asm(nop);&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;IBCR = 0; //Stop Transmission.&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any Suggestions would be greatly appreciated. Thanks guys.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 03 Mar 2007 05:48:37 GMT</pubDate>
    <dc:creator>chuckles</dc:creator>
    <dc:date>2007-03-03T05:48:37Z</dc:date>
    <item>
      <title>HC12 IIC - Need help</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HC12-IIC-Need-help/m-p/124917#M219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I need some pointers/help in using IIC bus.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm using it to send data to a serial DAC (Max521), which is compatible with IIC. However, when I run my code I'm not convinced that&amp;nbsp;it is outputting the correct wave forms...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The code is something like this:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;for(;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif"&gt;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/A&gt; {&lt;BR /&gt;&amp;nbsp;init_IIC();&lt;BR /&gt;&amp;nbsp;write_IIC();&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;}&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;void init_IIC(){&lt;BR /&gt;&amp;nbsp;//Try Setting DDRJ&lt;BR /&gt;&amp;nbsp;DDRJ_DDRJ6=1;&lt;BR /&gt;&amp;nbsp;DDRJ_DDRJ7=1;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;IBFD = 0x20;&amp;nbsp; //Frequency divider&lt;BR /&gt;&amp;nbsp;IBAD = 0x1F;&amp;nbsp; //This is to set the slave address of the IIC&amp;nbsp; -- Doesn't really matter&amp;nbsp;?&lt;BR /&gt;&amp;nbsp;IBCR= 0xB0; //Enables, makes master, sets to transmit&lt;BR /&gt;&amp;nbsp;&amp;nbsp;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;void write_IIC() {&lt;BR /&gt;&amp;nbsp;IBDR = 0x50; // Slave Address 0101 0000&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;while(IBSR_TCF ==0 ) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;asm(nop);&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;IBDR= 0x00; //DAC0&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;while(IBSR_TCF ==0 ) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;asm(nop);&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;IBDR = 0xFF;//Activate DAC full tilt&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;while(IBSR_TCF ==0 ) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;asm(nop);&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;IBCR = 0; //Stop Transmission.&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any Suggestions would be greatly appreciated. Thanks guys.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Mar 2007 05:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HC12-IIC-Need-help/m-p/124917#M219</guid>
      <dc:creator>chuckles</dc:creator>
      <dc:date>2007-03-03T05:48:37Z</dc:date>
    </item>
    <item>
      <title>Re: HC12 IIC - Need help</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HC12-IIC-Need-help/m-p/124918#M220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Try change your code for this&lt;BR /&gt;&lt;BR /&gt;void write_IIC() {&lt;BR /&gt;&amp;nbsp;IBDR = 0x50; // Slave Address 0101 0000&lt;BR /&gt;&lt;BR /&gt;//wait until transfer all byte&lt;BR /&gt;&amp;nbsp;while(!IBSR_IBIF);&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;//clear flag&lt;BR /&gt;&amp;nbsp;IBSR_IBIF = 1;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Check ACK&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(IBSR_RXACK)&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; //if this bit its set, the device not response&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; _asm nop;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //include here something&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; _asm nop;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; //All OK, your DAC response to Address call&lt;BR /&gt;&amp;nbsp;}&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2007 22:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/HC12-IIC-Need-help/m-p/124918#M220</guid>
      <dc:creator>erooll</dc:creator>
      <dc:date>2007-06-14T22:48:13Z</dc:date>
    </item>
  </channel>
</rss>