<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: XGATE Warning A22011 Operand out of range in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2195333#M20769</link>
    <description>&lt;P&gt;Hi Ladisalv,&lt;/P&gt;&lt;P&gt;Excellent! That was what I needed. I studied your code and it made sense to me . I incorporated it into a basic test code and it worked as expected. I experimented with it a bit and that also worked as expected.&lt;/P&gt;&lt;P&gt;Thanks so much for giving me that clue to the puzzle.&lt;/P&gt;&lt;P&gt;Now, I have one more related related question about XGATE semaphores, but I think it would be better protocol to start and new thread, which I will do.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks again for your help, I don't know if I could have figured it out on my own or not.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Robert.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 30 Oct 2025 00:59:50 GMT</pubDate>
    <dc:creator>roberthiebert</dc:creator>
    <dc:date>2025-10-30T00:59:50Z</dc:date>
    <item>
      <title>XGATE Warning A22011 Operand out of range</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2192227#M20758</link>
      <description>&lt;P&gt;MC9S12XEP100, CW Special edition, relocatable assembler, dual processor, XGATE in RAM.&lt;/P&gt;&lt;P&gt;I'm having some success in my project getting XGATE to handle some of the interrupts, but I've run into an interesting problem. Things worked well until I started adding more shared variables. At one point I got the warning "A22011 Operand out of range".&lt;/P&gt;&lt;P&gt;My project is getting fairly big and complex so I just made a short test program to re-create the problem. The program is just the Fibo one that the wizard puts together with some more shared variables added. Up to 16 word variables is fine, after that it I get the warning and when I run the program the variables beyond 16 don't update.&lt;/P&gt;&lt;P&gt;I have no idea how to fix this. Any suggestions would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;</description>
      <pubDate>Fri, 24 Oct 2025 03:51:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2192227#M20758</guid>
      <dc:creator>roberthiebert</dc:creator>
      <dc:date>2025-10-24T03:51:04Z</dc:date>
    </item>
    <item>
      <title>Re: XGATE Warning A22011 Operand out of range</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2192897#M20760</link>
      <description>&lt;P&gt;I've been doing some more troubleshooting on this, reading the manuals, studying the PRM and .map files and using the debugger. I am using non-paged RAM and non-banked Flash.&lt;/P&gt;&lt;P&gt;The manual tells me that XGATE register R1 is preloaded with the initial pointer of the channel's service request vector. XGATE register R7 is preloaded with either the contents of XG1SP74 or XG1SP31.&lt;/P&gt;&lt;P&gt;Using the de-bugger I can see that the the linker has placed the shared variables&amp;nbsp; starting at address XGATE $E100. Addresses XGATE $E100 to $FFFF correspond to logical addresses $2100 to $3FFF.&lt;/P&gt;&lt;P&gt;With R1 containing $E100 I can only access 16 variables before I get and "out of range " error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In my project I eventually want XGATE to handle 27 different interrupt routines. One of which has to use a 256 byte lookup table.&lt;/P&gt;&lt;P&gt;Any suggestions on how I can handle this issue would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;</description>
      <pubDate>Sat, 25 Oct 2025 18:12:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2192897#M20760</guid>
      <dc:creator>roberthiebert</dc:creator>
      <dc:date>2025-10-25T18:12:48Z</dc:date>
    </item>
    <item>
      <title>Re: XGATE Warning A22011 Operand out of range</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2192921#M20761</link>
      <description>&lt;P&gt;Oops. Error on last post. Should be 32 variables (16 words), not 16 variables.&lt;/P&gt;</description>
      <pubDate>Sun, 26 Oct 2025 02:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2192921#M20761</guid>
      <dc:creator>roberthiebert</dc:creator>
      <dc:date>2025-10-26T02:22:45Z</dc:date>
    </item>
    <item>
      <title>Re: XGATE Warning A22011 Operand out of range</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2193578#M20763</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The question I have is &amp;gt; What do you want to do....&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;LDW R2,(R1,#(XGATE_CounterXX - MyData)) ; load counter&lt;BR /&gt;INC R2&lt;BR /&gt;STW R2,(R1,#(XGATE_CounterXX - MyData)) ; store counter&lt;BR /&gt;&lt;BR /&gt;Is that right you want to get a value from&amp;nbsp;XGATE_CounterXX, increment it and then put it back?&lt;BR /&gt;Or do you want to get an offset of the XGATE_CounterXX from MyData, incremnt it and put the value to the XGATE_CounterXX?&lt;BR /&gt;Or....?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 14:41:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2193578#M20763</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2025-10-27T14:41:58Z</dc:date>
    </item>
    <item>
      <title>Re: XGATE Warning A22011 Operand out of range</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2193583#M20764</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;having read last update I started to be more confused.&lt;BR /&gt;Would not be easier to prepare c code example as a development platform.&lt;/P&gt;
&lt;P&gt;Moreover, think about xgate in flash and ram, or process basic functions on xgate and then call (continue) with the interrupt on CPU (it is also possible).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 14:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2193583#M20764</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2025-10-27T14:53:12Z</dc:date>
    </item>
    <item>
      <title>Re: XGATE Warning A22011 Operand out of range</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2193635#M20767</link>
      <description>&lt;P&gt;Hi Ladislav,&lt;/P&gt;&lt;P&gt;Thanks very much for having a look at my code.&lt;/P&gt;&lt;P&gt;In this test code I just want to load the contents of&amp;nbsp;&lt;SPAN&gt;XGATE_CounterXX, increment it and store it back into&amp;nbsp;XGATE_CounterXX. The code works fine until I get to&amp;nbsp;XGATE_Counter_17, then I get the out of range error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It would be preferable if I could get the value from&amp;nbsp;XGATE_Counter_17 (and on for more variables) by using the offset from the beginning of .data. I assumed that the command line&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LDW R2,(R1,#(XGATE_CounterXX - MyData)) did just that, but it seems to limit me to a maximum of 32 bytes or 16 words from the start of .data.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Just what is it that the command&amp;nbsp;LDW R2,(R1,#(XGATE_CounterXX - MyData)) does? I can't find any description of it in any of the information that I have.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If my interpretation of the manuals is correct, it is faster (more efficient?) to run XGATE out of RAM rather than Flash, and isn't that the&amp;nbsp; whole point of using XGATE to handle the interrupts?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Using "C" language for anything for me is not an option because I do not speak the language.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 16:17:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2193635#M20767</guid>
      <dc:creator>roberthiebert</dc:creator>
      <dc:date>2025-10-27T16:17:58Z</dc:date>
    </item>
    <item>
      <title>Re: XGATE Warning A22011 Operand out of range</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2195256#M20768</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I have forgotten….. The instruction you use in given form has offset of 5 bits long, represents number of bytes and you use words.&lt;BR /&gt;M[RB, #OFFS5] ⇒RD&lt;BR /&gt;So max offset is 32 bytes or 16 words.&lt;/P&gt;
&lt;P&gt;Look at this simple example of writing the Array of 256 words addressed by variable index.&lt;BR /&gt;Note that R0 is always 0.&lt;BR /&gt;XGATE_DATA: SECTION&lt;/P&gt;
&lt;P&gt;; put your variables here &lt;BR /&gt;ALIGN 2&lt;BR /&gt;Arr DS.W 256&lt;BR /&gt;Index DS.W 1&lt;/P&gt;
&lt;P&gt;XGATE_CODE: SECTION&lt;/P&gt;
&lt;P&gt;; interrupt handler for the software trigger 0&lt;BR /&gt;ALIGN 2&lt;BR /&gt;SoftwareTrigger0_Handler:&lt;/P&gt;
&lt;P&gt;; load index with value&lt;BR /&gt;LDW R2, Index ; Addr to Index&lt;BR /&gt;LDL R3, #17 ;&lt;BR /&gt;STW R3, (R2,R0) ; Save Index value &lt;BR /&gt;;-------------------------- Write Arr[5] = 0x1234&lt;BR /&gt;LDW R3, Index ; Get address of Index&lt;BR /&gt;; R3 = get address of index&lt;BR /&gt;LDW R2, (R3, R0) ; R2 = Index&lt;BR /&gt;LSL R2, #$1 ; Calculate Index in bytes; R2 = Index*2 data set is size of word &lt;BR /&gt;; Get position of Arr[Index]&lt;BR /&gt;LDW R3, Arr ; Base address of Addr&lt;BR /&gt;ADD R4, R2,R3 ; Calculate Arr[Index] position = Arr + Index*2&lt;BR /&gt;LDW R3, #$1234&lt;BR /&gt;STW R3, (R4, R0) ; Write Arr[Index] = $1234&lt;/P&gt;
&lt;P&gt;Note, in the memory window you will see Arr[0..512] (even we defined Arr DS.W 256) so writing word to arr index 17 will in reality write word to Arr[34] and arr[35] in memory window.&lt;/P&gt;
&lt;P&gt;Note that similar is read from the array.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you want to use instruction with #OFF5 then you can make something like addressing 2dimensional array of words which has elements [x,16]. But I see this as little bit complicated.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;L.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 16:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2195256#M20768</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2025-10-29T16:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: XGATE Warning A22011 Operand out of range</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2195333#M20769</link>
      <description>&lt;P&gt;Hi Ladisalv,&lt;/P&gt;&lt;P&gt;Excellent! That was what I needed. I studied your code and it made sense to me . I incorporated it into a basic test code and it worked as expected. I experimented with it a bit and that also worked as expected.&lt;/P&gt;&lt;P&gt;Thanks so much for giving me that clue to the puzzle.&lt;/P&gt;&lt;P&gt;Now, I have one more related related question about XGATE semaphores, but I think it would be better protocol to start and new thread, which I will do.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks again for your help, I don't know if I could have figured it out on my own or not.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Robert.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 00:59:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XGATE-Warning-A22011-Operand-out-of-range/m-p/2195333#M20769</guid>
      <dc:creator>roberthiebert</dc:creator>
      <dc:date>2025-10-30T00:59:50Z</dc:date>
    </item>
  </channel>
</rss>