<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: IIC Levels for S912ZVLA</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2140748#M20665</link>
    <description>thx</description>
    <pubDate>Fri, 25 Jul 2025 08:17:55 GMT</pubDate>
    <dc:creator>Boris_Bloxsberg</dc:creator>
    <dc:date>2025-07-25T08:17:55Z</dc:date>
    <item>
      <title>IIC Levels for S912ZVLA</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2140194#M20663</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;does some know the input levels for the IIC input of the&amp;nbsp;S912ZVLA.&lt;/P&gt;&lt;P&gt;I didn´t find this in the manual.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 24 Jul 2025 13:19:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2140194#M20663</guid>
      <dc:creator>Boris_Bloxsberg</dc:creator>
      <dc:date>2025-07-24T13:19:24Z</dc:date>
    </item>
    <item>
      <title>Re: IIC Levels for S912ZVLA</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2140686#M20664</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The IIC input voltage levels for the&amp;nbsp;S912ZVLA&amp;nbsp;microcontroller are not explicitly listed but they are typically defined by the&amp;nbsp;digital input thresholds&amp;nbsp;for the I/O pins used for SDA and SCL.&lt;/P&gt;
&lt;P&gt;Typical IIC Pin Thresholds:&lt;/P&gt;
&lt;P&gt;For&amp;nbsp;5V-tolerant I/O&amp;nbsp;(which is common in the S12Z family), the input high voltage (VIH) is typically&amp;nbsp;&lt;/P&gt;
&lt;P&gt;0.65 × VDDx&amp;nbsp;and the input low voltage (VIL) is&amp;nbsp;0.35 * VDDx.&lt;/P&gt;
&lt;P&gt;If VDDx = 5V, then guarenteed value:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;VIH&amp;gt;= 3.25V (minimum to be recognized as HIGH)&lt;/LI&gt;
&lt;LI&gt;VIL &amp;lt;= 1.75V (maximum to be recognized as LOW)&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Of course, real threshold value is somewhere between (1.75 + 125 mV) and ( 3.25 - 125 mV) considering 250mV hysteresis connected to this threshold for changes between log.0 and log.1&lt;/P&gt;
&lt;P&gt;For example&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lama_0-1753426926938.jpeg" style="width: 660px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/349468iF06DDF56DD3C0720/image-dimensions/660x495?v=v2" width="660" height="495" role="button" title="lama_0-1753426926938.jpeg" alt="lama_0-1753426926938.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lama_0-1753426926938.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jul 2025 07:25:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2140686#M20664</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2025-07-25T07:25:39Z</dc:date>
    </item>
    <item>
      <title>Re: IIC Levels for S912ZVLA</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2140748#M20665</link>
      <description>thx</description>
      <pubDate>Fri, 25 Jul 2025 08:17:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2140748#M20665</guid>
      <dc:creator>Boris_Bloxsberg</dc:creator>
      <dc:date>2025-07-25T08:17:55Z</dc:date>
    </item>
    <item>
      <title>Re: IIC Levels for S912ZVLA</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2142343#M20673</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Yeah, those VIH/VIL numbers for the S12Z family are pretty standard, especially for 5V-tolerant I/O. Just remember that hysteresis helps a lot with noise, but you&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;really&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;want to&amp;nbsp; &lt;A href="https://driftboss3d.io" target="_self"&gt;Drift Boss&lt;/A&gt; make sure your I2C signals are clean and the pull-ups are strong enough, or you’ll chase ghost errors for hours.&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Tue, 29 Jul 2025 06:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2142343#M20673</guid>
      <dc:creator>barkerxavierr</dc:creator>
      <dc:date>2025-07-29T06:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: IIC Levels for S912ZVLA</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2157443#M20710</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The only issue I see in the internal pull up. They are really weak 20kohm-50kohm. I suggest to use external ones 1k~10k.&lt;/P&gt;
&lt;P&gt;Always use external pull-up resistors (typically 4.7kΩ is a good starting point).&lt;/P&gt;
&lt;P&gt;You can leave internal pull-ups disabled, or enable them as a backup — but don’t rely on them for I²C operation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 25 Aug 2025 08:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IIC-Levels-for-S912ZVLA/m-p/2157443#M20710</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2025-08-25T08:47:25Z</dc:date>
    </item>
  </channel>
</rss>