<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: S12z linker symbol creation</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12z-linker-symbol-creation/m-p/2095533#M20472</link>
    <description>&lt;P&gt;Thanks Daniel,&lt;/P&gt;&lt;P&gt;This solution is great!&lt;/P&gt;&lt;P&gt;Regards&lt;BR /&gt;tomrix&lt;/P&gt;</description>
    <pubDate>Mon, 12 May 2025 13:23:20 GMT</pubDate>
    <dc:creator>tomrix</dc:creator>
    <dc:date>2025-05-12T13:23:20Z</dc:date>
    <item>
      <title>S12z linker symbol creation</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12z-linker-symbol-creation/m-p/2094744#M20469</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to implement a stack usage supervision by iitializing the stack with a pattern and then check it cyclically.&lt;/P&gt;&lt;P&gt;I can find the linker symbol&amp;nbsp;__SEG_END_SSTACK but no stack size or stack start address symbol is generated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone help on how to tell the linker to create such a symbol?&lt;/P&gt;&lt;P&gt;Regards&lt;BR /&gt;tomrix&lt;/P&gt;</description>
      <pubDate>Fri, 09 May 2025 16:48:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12z-linker-symbol-creation/m-p/2094744#M20469</guid>
      <dc:creator>tomrix</dc:creator>
      <dc:date>2025-05-09T16:48:36Z</dc:date>
    </item>
    <item>
      <title>Re: S12z linker symbol creation</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12z-linker-symbol-creation/m-p/2095522#M20471</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247888"&gt;@tomrix&lt;/a&gt;.,&lt;/P&gt;
&lt;P&gt;There is a workaround to fill the stack with known values.&lt;BR /&gt;Please refer to the attached test project.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;In the .prm linker file, there are two RAM sections.&lt;BR /&gt;The MY_STACK section is used for the Stack and it is filled with 0xED.&lt;BR /&gt;While the rest of RAM is filled with 0xAB.&lt;BR /&gt;The STACKTOP is then placed at the end of MY_STACK section.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1747054985589.png" style="width: 1006px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/337217i64E8B88361E855FF/image-dimensions/1006x445?v=v2" width="1006" height="445" role="button" title="danielmartynek_0-1747054985589.png" alt="danielmartynek_0-1747054985589.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 May 2025 13:03:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12z-linker-symbol-creation/m-p/2095522#M20471</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-05-12T13:03:32Z</dc:date>
    </item>
    <item>
      <title>Re: S12z linker symbol creation</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12z-linker-symbol-creation/m-p/2095533#M20472</link>
      <description>&lt;P&gt;Thanks Daniel,&lt;/P&gt;&lt;P&gt;This solution is great!&lt;/P&gt;&lt;P&gt;Regards&lt;BR /&gt;tomrix&lt;/P&gt;</description>
      <pubDate>Mon, 12 May 2025 13:23:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12z-linker-symbol-creation/m-p/2095533#M20472</guid>
      <dc:creator>tomrix</dc:creator>
      <dc:date>2025-05-12T13:23:20Z</dc:date>
    </item>
  </channel>
</rss>