<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 MagniV S12ZVM VREG temperature sensor</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVM-VREG-temperature-sensor/m-p/2065588#M20398</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a project with the&amp;nbsp;S912ZVMC12F3 MCU.&lt;/P&gt;&lt;P&gt;In the reference manual revision 2.15 (5.9.2023) I can find the calculation for the internal temperature sensore VHT / VREG:&lt;BR /&gt;VHT(temp) = VHT(150) - (150 - temp) * dVHT&lt;BR /&gt;VHT(150) = 2,4 V&lt;BR /&gt;dVHT = 5,25 mv/°C typical&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/435"&gt;@RT&lt;/a&gt; I measure a value of ~1342 =&amp;gt; ~5°C which is obviously not correct.&lt;/P&gt;&lt;P&gt;When checking an older version of the reference manual (Rev. 1.4 22.5.2014) I can find the following values:&lt;BR /&gt;VHT(150) = 2,25 V&lt;BR /&gt;dVHT = 5,05 mv/°C typical&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/435"&gt;@RT&lt;/a&gt; ~1342 =&amp;gt; ~29°C which is more plausible (but still a bit too high as it is winter and my colleague always wants to keep the window open so it is acutally more like &amp;lt;20°C :D)&lt;/P&gt;&lt;P&gt;Can you please help out on what are the correct values to be used?&lt;/P&gt;&lt;P&gt;Kind regards&lt;BR /&gt;tomrix&lt;/P&gt;</description>
    <pubDate>Thu, 20 Mar 2025 12:59:24 GMT</pubDate>
    <dc:creator>tomrix</dc:creator>
    <dc:date>2025-03-20T12:59:24Z</dc:date>
    <item>
      <title>MagniV S12ZVM VREG temperature sensor</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVM-VREG-temperature-sensor/m-p/2065588#M20398</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a project with the&amp;nbsp;S912ZVMC12F3 MCU.&lt;/P&gt;&lt;P&gt;In the reference manual revision 2.15 (5.9.2023) I can find the calculation for the internal temperature sensore VHT / VREG:&lt;BR /&gt;VHT(temp) = VHT(150) - (150 - temp) * dVHT&lt;BR /&gt;VHT(150) = 2,4 V&lt;BR /&gt;dVHT = 5,25 mv/°C typical&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/435"&gt;@RT&lt;/a&gt; I measure a value of ~1342 =&amp;gt; ~5°C which is obviously not correct.&lt;/P&gt;&lt;P&gt;When checking an older version of the reference manual (Rev. 1.4 22.5.2014) I can find the following values:&lt;BR /&gt;VHT(150) = 2,25 V&lt;BR /&gt;dVHT = 5,05 mv/°C typical&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/435"&gt;@RT&lt;/a&gt; ~1342 =&amp;gt; ~29°C which is more plausible (but still a bit too high as it is winter and my colleague always wants to keep the window open so it is acutally more like &amp;lt;20°C :D)&lt;/P&gt;&lt;P&gt;Can you please help out on what are the correct values to be used?&lt;/P&gt;&lt;P&gt;Kind regards&lt;BR /&gt;tomrix&lt;/P&gt;</description>
      <pubDate>Thu, 20 Mar 2025 12:59:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVM-VREG-temperature-sensor/m-p/2065588#M20398</guid>
      <dc:creator>tomrix</dc:creator>
      <dc:date>2025-03-20T12:59:24Z</dc:date>
    </item>
    <item>
      <title>Re: MagniV S12ZVM VREG temperature sensor</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVM-VREG-temperature-sensor/m-p/2066395#M20400</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN3624.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN3624.pdf&lt;/A&gt; ... Uses also old values of dVht, originally designed for S12ZVC and first versions.&lt;/P&gt;
&lt;P&gt;The change was done &lt;STRONG&gt;Table 0-1. Revision History:&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;14 DEC 2015 2.4&lt;/P&gt;
&lt;P&gt;Updated temperature sensor electrical specification, Table B-1&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So the latest version provides the values ​​we currently guarantee.&lt;/P&gt;
&lt;P&gt;However, as an design engineer I would use the worst case scenario which provides me safety range.&lt;/P&gt;
&lt;P&gt;I can not imagine you will perform trimming for each device separately. But I can be wrong.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Fri, 21 Mar 2025 15:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MagniV-S12ZVM-VREG-temperature-sensor/m-p/2066395#M20400</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2025-03-21T15:00:47Z</dc:date>
    </item>
  </channel>
</rss>