<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Codewarrior : Facing issue in Automation using TCL Scripting</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Codewarrior-Facing-issue-in-Automation-using-TCL-Scripting/m-p/2064631#M20396</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I found an automation guide (&lt;SPAN&gt;&lt;A title="https://www.nxp.com/docs/en/user-guide/ide_5.6_automation_guide.pdf" href="https://www.nxp.com/docs/en/user-guide/IDE_5.6_Automation_Guide.pdf" target="_blank" rel="noreferrer noopener"&gt;https://www.nxp.com/docs/en/user-guide/IDE_5.6_Automation_Guide.pdf&lt;/A&gt;) which states that TCL scripts can be used for automating flashing and debugging operations and found it quite useful but facing some challenge/issue as well i.e. once the flashing is completed, need to quit/close the CodeWarrior IDE. Document recommends to use "quitIDE" command for the same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Used the same command but it closes only one thread of the CodeWarrior IDE i.e. closes the IDE&amp;nbsp; but respective process/thread still exists/visible in the Task Manager window. I need to close the same forcefully.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Looking for some idea/thought through which Codewarrior IDE can be closed completely.&lt;/P&gt;</description>
    <pubDate>Wed, 19 Mar 2025 10:38:41 GMT</pubDate>
    <dc:creator>in-nitin-gupta</dc:creator>
    <dc:date>2025-03-19T10:38:41Z</dc:date>
    <item>
      <title>Codewarrior : Facing issue in Automation using TCL Scripting</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Codewarrior-Facing-issue-in-Automation-using-TCL-Scripting/m-p/2064631#M20396</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I found an automation guide (&lt;SPAN&gt;&lt;A title="https://www.nxp.com/docs/en/user-guide/ide_5.6_automation_guide.pdf" href="https://www.nxp.com/docs/en/user-guide/IDE_5.6_Automation_Guide.pdf" target="_blank" rel="noreferrer noopener"&gt;https://www.nxp.com/docs/en/user-guide/IDE_5.6_Automation_Guide.pdf&lt;/A&gt;) which states that TCL scripts can be used for automating flashing and debugging operations and found it quite useful but facing some challenge/issue as well i.e. once the flashing is completed, need to quit/close the CodeWarrior IDE. Document recommends to use "quitIDE" command for the same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Used the same command but it closes only one thread of the CodeWarrior IDE i.e. closes the IDE&amp;nbsp; but respective process/thread still exists/visible in the Task Manager window. I need to close the same forcefully.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Looking for some idea/thought through which Codewarrior IDE can be closed completely.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 10:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Codewarrior-Facing-issue-in-Automation-using-TCL-Scripting/m-p/2064631#M20396</guid>
      <dc:creator>in-nitin-gupta</dc:creator>
      <dc:date>2025-03-19T10:38:41Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior : Facing issue in Automation using TCL Scripting</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Codewarrior-Facing-issue-in-Automation-using-TCL-Scripting/m-p/2069501#M20412</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm not much familiar with CW v5.6 and it's scripting language. But if the the tcl console allows call OS commands, you can use taskkill command.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When I went through the guide, may be the quitIDE will work if you start new IDE for the console with&amp;nbsp;/s&amp;nbsp; parameter.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Mar 2025 13:42:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Codewarrior-Facing-issue-in-Automation-using-TCL-Scripting/m-p/2069501#M20412</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2025-03-27T13:42:48Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior : Facing issue in Automation using TCL Scripting</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Codewarrior-Facing-issue-in-Automation-using-TCL-Scripting/m-p/2071044#M20415</link>
      <description>&lt;P&gt;Hi Jira_kral&lt;/P&gt;&lt;P&gt;Thanks for your reply.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Well as soon as I execute quitIDE, there is no console to execute "taskkill" command. Also if I try to execute through the dos prompt then it is hard to gauge the completion of the existing TCL scripting. I mean there needs to be a sync between TCL Script and External DOS command execution for "task kill".&lt;/P&gt;</description>
      <pubDate>Mon, 31 Mar 2025 10:08:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Codewarrior-Facing-issue-in-Automation-using-TCL-Scripting/m-p/2071044#M20415</guid>
      <dc:creator>in-nitin-gupta</dc:creator>
      <dc:date>2025-03-31T10:08:04Z</dc:date>
    </item>
  </channel>
</rss>