<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: S12Z Reset only to Normal Chip Mode</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-Reset-only-to-Normal-Chip-Mode/m-p/2061216#M20390</link>
    <description>&lt;P&gt;I understand your explanation, but then what is the purpose of this setting&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="manishsangram_0-1741861249384.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/327958iBA460222112045BA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="manishsangram_0-1741861249384.png" alt="manishsangram_0-1741861249384.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;manishsangram_0-1741861249384.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And operating mode switching means what?&lt;/P&gt;</description>
    <pubDate>Thu, 13 Mar 2025 10:21:57 GMT</pubDate>
    <dc:creator>manishsangram</dc:creator>
    <dc:date>2025-03-13T10:21:57Z</dc:date>
    <item>
      <title>S12Z Reset only to Normal Chip Mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-Reset-only-to-Normal-Chip-Mode/m-p/2058306#M20374</link>
      <description>&lt;P&gt;As per the&amp;nbsp;MC9S12ZVM Family Reference Manual Rev 2.15&lt;/P&gt;&lt;P&gt;Mode Select Bit — This bit determines the current operating mode of the MCU. Its reset value is captured from the MODC pin at the rising edge of the RESET pin.&lt;/P&gt;&lt;P&gt;I am a bit confused and am seeking clarification here&lt;/P&gt;&lt;P&gt;1. In CodeWarrior when I change the "Boot Operating Mode" where is the change made in code or configuration? I assume it has to be made in the debugger profile, but I can't find it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. If the device is secure and the Boot Mode was set to "Normal" when code was flashed. Will subsequently reset with different MODC pin value allow switching to Special mode and allow debug access?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 09 Mar 2025 15:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-Reset-only-to-Normal-Chip-Mode/m-p/2058306#M20374</guid>
      <dc:creator>manishsangram</dc:creator>
      <dc:date>2025-03-09T15:09:42Z</dc:date>
    </item>
    <item>
      <title>Re: S12Z Reset only to Normal Chip Mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-Reset-only-to-Normal-Chip-Mode/m-p/2058730#M20377</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1) CodeWarrior considers you are using debugger so the multilink automatically ties the MODC pin to 0. You can also see that MODC pin has internal pull-up device connected during reset. Also, there is normal in the HW design to have MODC pin connected to the 3.3k or 4.7k pull-up resistor.&lt;/P&gt;
&lt;P&gt;Any reset which is not initiated by debug interface for load/debug purposes is then started in the normal mode. For example power on, reset button pressing, …&lt;/P&gt;
&lt;P&gt;Of course, if the device is secured the MCU goes into the special mode when debugger tries to connect but the only mass erase command is available.&lt;/P&gt;
&lt;P&gt;2) As I wrote above. Normal mode is selected by MODC pin value during reset. If you reset the MCU to a special mode secured MCU is not accessible and the only mass erase command is available&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Note, standard problem of understanding normal and special mode is when some registers are write once or not accessible in normal mode and accessible or rewritable anytime in special mode.&lt;/P&gt;
&lt;P&gt;Debug mode (special mode) enables you to perform you some action which are not allowed in normal mode.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 10 Mar 2025 11:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-Reset-only-to-Normal-Chip-Mode/m-p/2058730#M20377</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2025-03-10T11:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: S12Z Reset only to Normal Chip Mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-Reset-only-to-Normal-Chip-Mode/m-p/2061216#M20390</link>
      <description>&lt;P&gt;I understand your explanation, but then what is the purpose of this setting&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="manishsangram_0-1741861249384.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/327958iBA460222112045BA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="manishsangram_0-1741861249384.png" alt="manishsangram_0-1741861249384.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;manishsangram_0-1741861249384.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And operating mode switching means what?&lt;/P&gt;</description>
      <pubDate>Thu, 13 Mar 2025 10:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-Reset-only-to-Normal-Chip-Mode/m-p/2061216#M20390</guid>
      <dc:creator>manishsangram</dc:creator>
      <dc:date>2025-03-13T10:21:57Z</dc:date>
    </item>
  </channel>
</rss>