<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S912ZVMC12F3 HAL/MCAL drivers in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVMC12F3-HAL-MCAL-drivers/m-p/2059407#M20379</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently starting a project with a S912ZVMC12F3 controller and I was wondering if there are Hardware Abstraction Layer (HAL) drivers / MCALs provided by NXP?&lt;/P&gt;&lt;P&gt;According to table at&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/automotive-software-and-tools/autosar:AUTOSAR-HOME" target="_self"&gt;AUTOSAR® Software Architecture | NXP Semiconductors&lt;/A&gt;&amp;nbsp;there are MCALS available, but not for S12Z MCUs.&amp;nbsp;&lt;BR /&gt;&lt;SPAN&gt;For S12ZVMC256 MagniV MCUs it is provided, so I was also wondering whether it can be used as the MCU is similar??&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Appreciate support, cheers Thomas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 11 Mar 2025 09:52:15 GMT</pubDate>
    <dc:creator>tomrix</dc:creator>
    <dc:date>2025-03-11T09:52:15Z</dc:date>
    <item>
      <title>S912ZVMC12F3 HAL/MCAL drivers</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVMC12F3-HAL-MCAL-drivers/m-p/2059407#M20379</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently starting a project with a S912ZVMC12F3 controller and I was wondering if there are Hardware Abstraction Layer (HAL) drivers / MCALs provided by NXP?&lt;/P&gt;&lt;P&gt;According to table at&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/automotive-software-and-tools/autosar:AUTOSAR-HOME" target="_self"&gt;AUTOSAR® Software Architecture | NXP Semiconductors&lt;/A&gt;&amp;nbsp;there are MCALS available, but not for S12Z MCUs.&amp;nbsp;&lt;BR /&gt;&lt;SPAN&gt;For S12ZVMC256 MagniV MCUs it is provided, so I was also wondering whether it can be used as the MCU is similar??&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Appreciate support, cheers Thomas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Mar 2025 09:52:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVMC12F3-HAL-MCAL-drivers/m-p/2059407#M20379</guid>
      <dc:creator>tomrix</dc:creator>
      <dc:date>2025-03-11T09:52:15Z</dc:date>
    </item>
    <item>
      <title>Re: S912ZVMC12F3 HAL/MCAL drivers</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVMC12F3-HAL-MCAL-drivers/m-p/2060534#M20388</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247888"&gt;@tomrix&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;According to the release notes of the MCAL drivers, only the S12ZVMC256 is supported.&lt;/P&gt;
&lt;P&gt;As you said, the MCUs are very similar - most of the modules like SPI, SCI, MSCAN are the same.&lt;/P&gt;
&lt;P&gt;But there are differences too, refer to the RM, Table 1-3. S12ZVM Module Version Table.&lt;/P&gt;
&lt;P&gt;Also, in general, the MCAL drivers requires more Flash and SRAM. &lt;/P&gt;
&lt;P&gt;There is only 8kB of SRAM and 128kB of Flash on S12ZVMC12.&lt;/P&gt;
&lt;P&gt;The MCAL comes with a Quality package that has Memory size reports for each driver.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Mar 2025 14:50:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912ZVMC12F3-HAL-MCAL-drivers/m-p/2060534#M20388</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-03-12T14:50:20Z</dc:date>
    </item>
  </channel>
</rss>