<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: Radar Dataset Adaptation_S32R274 Development Board</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Radar-Dataset-Adaptation-S32R274-Development-Board/m-p/2037178#M20333</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for reply!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, exactly. So, I stored some raw data taken from the sensor on my PC. Now I wanna input it to the micro, process it and then visualize it on the PC similar to the&amp;nbsp;OneRF_4Antennas_demo_s32r274 example.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Hadi&lt;/P&gt;</description>
    <pubDate>Mon, 03 Feb 2025 11:40:53 GMT</pubDate>
    <dc:creator>HaMun</dc:creator>
    <dc:date>2025-02-03T11:40:53Z</dc:date>
    <item>
      <title>Radar Dataset Adaptation_S32R274 Development Board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Radar-Dataset-Adaptation-S32R274-Development-Board/m-p/2036562#M20329</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I ran the&amp;nbsp;OneRF_4Antennas_demo_s32r274 example (able to compile, build it). Since I don't have the radar sensor TEF810X on board&amp;nbsp;I was not able to visualize it. I would like to run the same example with my own radar data (which is raw radar data) stored a host computer and would like to transmit this data via Ethernet to the Board(S32R272) something like this&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/321997iAFA5F1CD2F9682D1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I would like to do the same processing performed in the example and visualize the output similar to the example as well. I would appreciate it if you could guide over this ?&lt;BR /&gt;&lt;BR /&gt;Best,&lt;/P&gt;&lt;P&gt;Hadi&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jan 2025 12:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Radar-Dataset-Adaptation-S32R274-Development-Board/m-p/2036562#M20329</guid>
      <dc:creator>HaMun</dc:creator>
      <dc:date>2025-01-31T12:07:16Z</dc:date>
    </item>
    <item>
      <title>Re: Radar Dataset Adaptation_S32R274 Development Board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Radar-Dataset-Adaptation-S32R274-Development-Board/m-p/2037172#M20332</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;so you would like to input raw data from your PC to uC at the point where raw data are coming from sensor?&lt;/P&gt;
&lt;P&gt;and then process them on uC and visualize on your PC. Correct?&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Mon, 03 Feb 2025 11:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Radar-Dataset-Adaptation-S32R274-Development-Board/m-p/2037172#M20332</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-02-03T11:23:21Z</dc:date>
    </item>
    <item>
      <title>Re: Radar Dataset Adaptation_S32R274 Development Board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Radar-Dataset-Adaptation-S32R274-Development-Board/m-p/2037178#M20333</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for reply!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, exactly. So, I stored some raw data taken from the sensor on my PC. Now I wanna input it to the micro, process it and then visualize it on the PC similar to the&amp;nbsp;OneRF_4Antennas_demo_s32r274 example.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Hadi&lt;/P&gt;</description>
      <pubDate>Mon, 03 Feb 2025 11:40:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Radar-Dataset-Adaptation-S32R274-Development-Board/m-p/2037178#M20333</guid>
      <dc:creator>HaMun</dc:creator>
      <dc:date>2025-02-03T11:40:53Z</dc:date>
    </item>
    <item>
      <title>Re: Radar Dataset Adaptation_S32R274 Development Board</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Radar-Dataset-Adaptation-S32R274-Development-Board/m-p/2037553#M20334</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I have asked RADAR team to comment on this thread:&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;I have looked at it. It seems a pretty straightforward re-use of the software components in the demo project, in particular the Ethernet driver. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;You should modify the application to use Ethernet instead of MIPI to receive the radar data and fill the input buffer for the radar processing sequence.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;Peter&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 07:20:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Radar-Dataset-Adaptation-S32R274-Development-Board/m-p/2037553#M20334</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-02-04T07:20:46Z</dc:date>
    </item>
  </channel>
</rss>