<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PP4/PW4 pin in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/PP4-PW4-pin/m-p/2021377#M20281</link>
    <description>&lt;P&gt;Hello newbie here,&lt;/P&gt;&lt;P&gt;I'm looking at a mc9s12gc (52 pin) on HVAC board and noticed that a Thermostat(Basically a potentiometer) what I would think should be tied to an input pin is wired to the PP4/PW4 pin. Can the PW4 pin be configured as an input? Everything I've read says it is a Pulse width modulated waveform output.&lt;/P&gt;&lt;P&gt;I know most thermostats are just open/closed contacts but this one is not.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 02 Jan 2025 16:54:25 GMT</pubDate>
    <dc:creator>P0zburn</dc:creator>
    <dc:date>2025-01-02T16:54:25Z</dc:date>
    <item>
      <title>PP4/PW4 pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/PP4-PW4-pin/m-p/2021377#M20281</link>
      <description>&lt;P&gt;Hello newbie here,&lt;/P&gt;&lt;P&gt;I'm looking at a mc9s12gc (52 pin) on HVAC board and noticed that a Thermostat(Basically a potentiometer) what I would think should be tied to an input pin is wired to the PP4/PW4 pin. Can the PW4 pin be configured as an input? Everything I've read says it is a Pulse width modulated waveform output.&lt;/P&gt;&lt;P&gt;I know most thermostats are just open/closed contacts but this one is not.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jan 2025 16:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/PP4-PW4-pin/m-p/2021377#M20281</guid>
      <dc:creator>P0zburn</dc:creator>
      <dc:date>2025-01-02T16:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: PP4/PW4 pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/PP4-PW4-pin/m-p/2021765#M20285</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245042"&gt;@P0zburn&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The PP4/PW4 pin is a GPIO.&lt;/P&gt;
&lt;P&gt;The direction is configurable in the DDRP register.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1735894186337.png" style="width: 620px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/318017iA005F1BE24CC5823/image-dimensions/620x344?v=v2" width="620" height="344" role="button" title="danielmartynek_0-1735894186337.png" alt="danielmartynek_0-1735894186337.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1735894186337.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jan 2025 08:50:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/PP4-PW4-pin/m-p/2021765#M20285</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-01-03T08:50:22Z</dc:date>
    </item>
    <item>
      <title>Re: PP4/PW4 pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/PP4-PW4-pin/m-p/2021990#M20292</link>
      <description>&lt;P&gt;Thanks for the response.&amp;nbsp; I have a follow up question. Once it is configured as an input, can it be used as a analog input?&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jan 2025 18:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/PP4-PW4-pin/m-p/2021990#M20292</guid>
      <dc:creator>P0zburn</dc:creator>
      <dc:date>2025-01-03T18:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: PP4/PW4 pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/PP4-PW4-pin/m-p/2022143#M20293</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245042"&gt;@P0zburn&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This is not an ATD (ADC) pin, it can be a digital input only.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1736112308677.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/318116i291371EAFA2E874B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielmartynek_0-1736112308677.png" alt="danielmartynek_0-1736112308677.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1736112308677.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Sun, 05 Jan 2025 21:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/PP4-PW4-pin/m-p/2022143#M20293</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-01-05T21:25:51Z</dc:date>
    </item>
  </channel>
</rss>