<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックIOC timer0/1 channels overflow flag</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IOC-timer0-1-channels-overflow-flag/m-p/1970266#M20180</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Micro: S12ZVCA192&lt;/P&gt;&lt;P&gt;For TIM 0/1 channels timer overflow,&amp;nbsp;TFLG2&amp;nbsp;TOF flag will get set. If we enable multiple channels of TIM0/1 at a time, How to find TFLG2&amp;nbsp;TOF flag is set because of which channel timer overflow?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Oct 2024 17:53:23 GMT</pubDate>
    <dc:creator>UmaMaheswaraReddy</dc:creator>
    <dc:date>2024-10-09T17:53:23Z</dc:date>
    <item>
      <title>IOC timer0/1 channels overflow flag</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IOC-timer0-1-channels-overflow-flag/m-p/1970266#M20180</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Micro: S12ZVCA192&lt;/P&gt;&lt;P&gt;For TIM 0/1 channels timer overflow,&amp;nbsp;TFLG2&amp;nbsp;TOF flag will get set. If we enable multiple channels of TIM0/1 at a time, How to find TFLG2&amp;nbsp;TOF flag is set because of which channel timer overflow?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 17:53:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IOC-timer0-1-channels-overflow-flag/m-p/1970266#M20180</guid>
      <dc:creator>UmaMaheswaraReddy</dc:creator>
      <dc:date>2024-10-09T17:53:23Z</dc:date>
    </item>
    <item>
      <title>Re: IOC timer0/1 channels overflow flag</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IOC-timer0-1-channels-overflow-flag/m-p/1971582#M20184</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Table 1-13. Interrupt Vector Locations&amp;nbsp;&amp;nbsp; (Reference Manual)&lt;/P&gt;
&lt;P&gt;Vector base + 0x1AC TIM0 timer overflow I bit TIM0TSCR2 (TOF) No Yes&lt;/P&gt;
&lt;P&gt;Vector base + 0x08C TIM1 timer overflow I bit TIM1TSCR2 (TOF) No Yes&lt;/P&gt;
&lt;P&gt;As you can see different vector number is used for the channels.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Moreover, 0x000F is an offset for the register TFLG2 for each timer.&lt;/P&gt;
&lt;P&gt;Exact address can be found:&lt;/P&gt;
&lt;P&gt;For&lt;/P&gt;
&lt;P&gt;TIM0: chapter: M.11 0x05C0-0x05EF TIM0&lt;/P&gt;
&lt;P&gt;TIM1: chapter M.8 0x0400-0x042F TIM1&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you use code warrior you van also check header file to get definition of the registers for given timer.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 18:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/IOC-timer0-1-channels-overflow-flag/m-p/1971582#M20184</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2024-10-10T18:33:37Z</dc:date>
    </item>
  </channel>
</rss>