<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックHow to revert applications in HCS12X?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-revert-applications-in-HCS12X/m-p/1899166#M19885</link>
    <description>&lt;P&gt;hello&lt;BR /&gt;Is there a way to revert the application during bootloader operation on the HCS12X series chip?&lt;BR /&gt;example:&lt;BR /&gt;- Unexpected interruption during flash erase in bootloader&lt;BR /&gt;- The application operates normally after reset&lt;BR /&gt;- Assuming that the application is already loaded&lt;BR /&gt;I can't seem to find the code in AN4258.&lt;/P&gt;</description>
    <pubDate>Thu, 04 Jul 2024 06:04:56 GMT</pubDate>
    <dc:creator>kuksu</dc:creator>
    <dc:date>2024-07-04T06:04:56Z</dc:date>
    <item>
      <title>How to revert applications in HCS12X?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-revert-applications-in-HCS12X/m-p/1899166#M19885</link>
      <description>&lt;P&gt;hello&lt;BR /&gt;Is there a way to revert the application during bootloader operation on the HCS12X series chip?&lt;BR /&gt;example:&lt;BR /&gt;- Unexpected interruption during flash erase in bootloader&lt;BR /&gt;- The application operates normally after reset&lt;BR /&gt;- Assuming that the application is already loaded&lt;BR /&gt;I can't seem to find the code in AN4258.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jul 2024 06:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-revert-applications-in-HCS12X/m-p/1899166#M19885</guid>
      <dc:creator>kuksu</dc:creator>
      <dc:date>2024-07-04T06:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to revert applications in HCS12X?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-revert-applications-in-HCS12X/m-p/1904338#M19920</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suggest to check CRC of the application before you jump into it to be sure it is OK.&lt;/P&gt;
&lt;P&gt;In the case you want to use, go back, into the original application than it is necessary to split flash into 2 spaces and use A/B swap method where new apps is switched to after it is chceck and we still have possibility to go to the previous apps. The issue of this method is the size of the memory.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jul 2024 12:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-revert-applications-in-HCS12X/m-p/1904338#M19920</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2024-07-09T12:31:51Z</dc:date>
    </item>
    <item>
      <title>Re: How to revert applications in HCS12X?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-revert-applications-in-HCS12X/m-p/1907033#M19956</link>
      <description>&lt;P&gt;In the end, it seems like there is only a dual bank method.&lt;BR /&gt;thank you&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 10:33:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/How-to-revert-applications-in-HCS12X/m-p/1907033#M19956</guid>
      <dc:creator>kuksu</dc:creator>
      <dc:date>2024-07-12T10:33:35Z</dc:date>
    </item>
  </channel>
</rss>