<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Bootloader reuse in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-reuse/m-p/1883530#M19860</link>
    <description>&lt;P&gt;The bootloader through CAN communication has been completed to some extent.&lt;/P&gt;&lt;P&gt;However, it can only be used once, so I would like to make it possible to re-enter the bootloader using any method.&lt;/P&gt;&lt;P&gt;The current progress order is bootloader- hex download via CAN GUI-download done-COP reset-Application run.&lt;/P&gt;&lt;P&gt;After running the application through COP reset, the application runs normally (LED, CAN ID communication).&lt;/P&gt;&lt;P&gt;The problem is that I can't re-enter the bootloader.&lt;/P&gt;&lt;P&gt;I tried accessing the switch using 4258SW's StartS12x.s, but it failed.&lt;/P&gt;&lt;P&gt;Please help with this issue, I would appreciate it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 07 Jun 2024 10:44:13 GMT</pubDate>
    <dc:creator>kuksu</dc:creator>
    <dc:date>2024-06-07T10:44:13Z</dc:date>
    <item>
      <title>Bootloader reuse</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-reuse/m-p/1883530#M19860</link>
      <description>&lt;P&gt;The bootloader through CAN communication has been completed to some extent.&lt;/P&gt;&lt;P&gt;However, it can only be used once, so I would like to make it possible to re-enter the bootloader using any method.&lt;/P&gt;&lt;P&gt;The current progress order is bootloader- hex download via CAN GUI-download done-COP reset-Application run.&lt;/P&gt;&lt;P&gt;After running the application through COP reset, the application runs normally (LED, CAN ID communication).&lt;/P&gt;&lt;P&gt;The problem is that I can't re-enter the bootloader.&lt;/P&gt;&lt;P&gt;I tried accessing the switch using 4258SW's StartS12x.s, but it failed.&lt;/P&gt;&lt;P&gt;Please help with this issue, I would appreciate it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jun 2024 10:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-reuse/m-p/1883530#M19860</guid>
      <dc:creator>kuksu</dc:creator>
      <dc:date>2024-06-07T10:44:13Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader reuse</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-reuse/m-p/1884255#M19864</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Switching between the bootloader and the application depends on the requirements of both parties involved. &lt;/SPAN&gt;&lt;SPAN&gt;The main problem seems to be that the bootloader requires a defined state, which in case of a complex application can be secured most simply by means of a reset, when we get all peripherals to the default state. &lt;/SPAN&gt;&lt;SPAN&gt;If we want to do it without a reset, then we have to ensure the compatibility and independent behavior of the bootloader and the application in such a way that they cannot be affected by any chance. &lt;/SPAN&gt;&lt;SPAN&gt;This problem is actually at the application level and does not concern technical support for the NXP product.&lt;/SPAN&gt;&lt;SPAN&gt; Unfortunately, we don't even have anything like that in the database of solved examples.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Ladislav&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jun 2024 13:04:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-reuse/m-p/1884255#M19864</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2024-06-10T13:04:37Z</dc:date>
    </item>
  </channel>
</rss>