<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックS12Z boot jump</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-boot-jump/m-p/1756576#M19515</link>
    <description>Debugging the boot of S12Z, but there was a problem with the boot redirecting to the app and it couldn't be redirected. Can you help me check the problem. My steps: 1. Boot burn address 0xFFC000-0xFFFDFF 2. APP burning address 0xFE0200-0xFFBFFF 3. The program runs in the boot to enable CAN_ IBS_ Control. u8con=2 to execute the jump app operation 4. The resulting program does not jump and runs directly into while (1) The attachment contains some code for the APP and boot project, and I have removed some other unrelated code</description>
    <pubDate>Tue, 14 Nov 2023 02:15:22 GMT</pubDate>
    <dc:creator>L_lh</dc:creator>
    <dc:date>2023-11-14T02:15:22Z</dc:date>
    <item>
      <title>S12Z boot jump</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-boot-jump/m-p/1756576#M19515</link>
      <description>Debugging the boot of S12Z, but there was a problem with the boot redirecting to the app and it couldn't be redirected. Can you help me check the problem. My steps: 1. Boot burn address 0xFFC000-0xFFFDFF 2. APP burning address 0xFE0200-0xFFBFFF 3. The program runs in the boot to enable CAN_ IBS_ Control. u8con=2 to execute the jump app operation 4. The resulting program does not jump and runs directly into while (1) The attachment contains some code for the APP and boot project, and I have removed some other unrelated code</description>
      <pubDate>Tue, 14 Nov 2023 02:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-boot-jump/m-p/1756576#M19515</guid>
      <dc:creator>L_lh</dc:creator>
      <dc:date>2023-11-14T02:15:22Z</dc:date>
    </item>
    <item>
      <title>Re: S12Z boot jump</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-boot-jump/m-p/1758246#M19518</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I'd like to suggest you to compare the code with this one....&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Simple-Serial-Bootloader-for-S12Z-AN-draft/ta-p/1126452" target="_blank"&gt;https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Simple-Serial-Bootloader-for-S12Z-AN-draft/ta-p/1126452&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladsialv&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 09:12:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-boot-jump/m-p/1758246#M19518</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2023-11-16T09:12:56Z</dc:date>
    </item>
  </channel>
</rss>