<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Floating VSS on S9S12G48F1</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1732033#M19471</link>
    <description>Hello again,&lt;BR /&gt;and thank you very much for the reply. I was kind of expecting something like that.&lt;BR /&gt;The question now is, how to best handle this situation? I cannot think of any test or detection method for this particular case.&lt;BR /&gt;&lt;BR /&gt;Any suggestions?&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;Vadim&lt;BR /&gt;&lt;BR /&gt;PS: It is a nice and vivid metaphor you used there, special thanks for that.</description>
    <pubDate>Fri, 29 Sep 2023 15:11:54 GMT</pubDate>
    <dc:creator>vadim_unterberg</dc:creator>
    <dc:date>2023-09-29T15:11:54Z</dc:date>
    <item>
      <title>Floating VSS on S9S12G48F1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1720182#M19434</link>
      <description>&lt;P&gt;Hello dear community,&lt;/P&gt;&lt;P&gt;I have a question, which came up during our failure simulation re-tests with the [S9S12G48F1MLC] microcontroller.&lt;/P&gt;&lt;P&gt;Removing the [Pin 5], which is the VSS (GND) connection of the device, does not cause any failures. The microcontroller sub-circuit continues to work without any issues.&lt;/P&gt;&lt;P&gt;The datasheet however clearly states in chapter [10.2.4],&amp;nbsp; that pin 5 has to be tied to GND.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So what happens, if the connection is removed due to a cold joint for example. There is no mention of that. My guess would be, that the µC finds itself an alternative GND. As far as I know, there are packages where VSS and VSSA are tied together internally, that should not be the case here. SO, either the external VSSA connection, or one of the grounded GPIOs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;- But is that supposed/allowed to happen?&lt;BR /&gt;- Does this damage the µC?&lt;BR /&gt;- Is there a way to avoid or detect this failure mode?&lt;/P&gt;&lt;P&gt;Any input or confirmation would be highly appreciated.&lt;/P&gt;&lt;P&gt;Bist regards&lt;BR /&gt;Vadim&lt;/P&gt;</description>
      <pubDate>Mon, 11 Sep 2023 08:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1720182#M19434</guid>
      <dc:creator>vadim_unterberg</dc:creator>
      <dc:date>2023-09-11T08:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: Floating VSS on S9S12G48F1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1720519#M19435</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;the connection to other VSS_ pins is performed also internally but not via wire but via ESD diode or some structures. The connection is not allowed to accept a load current so external connection to the GND MUST be done. Yes it can damage the MCU because it is a ticking time bomb with a random count down value.&lt;BR /&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 11 Sep 2023 16:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1720519#M19435</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2023-09-11T16:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: Floating VSS on S9S12G48F1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1732033#M19471</link>
      <description>Hello again,&lt;BR /&gt;and thank you very much for the reply. I was kind of expecting something like that.&lt;BR /&gt;The question now is, how to best handle this situation? I cannot think of any test or detection method for this particular case.&lt;BR /&gt;&lt;BR /&gt;Any suggestions?&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;Vadim&lt;BR /&gt;&lt;BR /&gt;PS: It is a nice and vivid metaphor you used there, special thanks for that.</description>
      <pubDate>Fri, 29 Sep 2023 15:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1732033#M19471</guid>
      <dc:creator>vadim_unterberg</dc:creator>
      <dc:date>2023-09-29T15:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: Floating VSS on S9S12G48F1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1732489#M19473</link>
      <description>&lt;P&gt;Hi Vadim,&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;for this case there is no suggestion except for the high quality of the soldering process.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;We really do not know about any workaround.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;Ladislav&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Oct 2023 08:58:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1732489#M19473</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2023-10-02T08:58:58Z</dc:date>
    </item>
    <item>
      <title>Re: Floating VSS on S9S12G48F1</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1733522#M19474</link>
      <description>Hello Again,&lt;BR /&gt;&lt;BR /&gt;that is unfortunate, but I have seen that coming.&amp;nbsp;&lt;BR /&gt;I guess the topic is closed then.&lt;BR /&gt;Thanks a lot for your input and with best regards,&lt;BR /&gt;&lt;BR /&gt;Vadim</description>
      <pubDate>Wed, 04 Oct 2023 06:11:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Floating-VSS-on-S9S12G48F1/m-p/1733522#M19474</guid>
      <dc:creator>vadim_unterberg</dc:creator>
      <dc:date>2023-10-04T06:11:03Z</dc:date>
    </item>
  </channel>
</rss>