<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックPort AD output on S9S12G</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Port-AD-output-on-S9S12G/m-p/1725555#M19458</link>
    <description>&lt;P&gt;Hi, I am having a problem with an S9S12G96, I have to use the AD port as output. On CODEWARRIOR Processor Expert correctly initializes the port:&lt;BR /&gt;MOVB #255,DDR0AD&lt;BR /&gt;MOVB #255,DDR1AD&lt;BR /&gt;I make it clear that I do not use these ports for anything else (ADC...)&lt;BR /&gt;The ADH and ADL ports seem to be configured as output, but I cannot control them... the lines:&lt;BR /&gt;MOVB #255, PT1AD&lt;BR /&gt;MOVB #255, PT0AD&lt;BR /&gt;Seem inoperable, outputs remain at 0&lt;BR /&gt;Someone ? to help me ?&lt;BR /&gt;THANKS !!!&lt;/P&gt;</description>
    <pubDate>Tue, 19 Sep 2023 13:40:39 GMT</pubDate>
    <dc:creator>Didier91</dc:creator>
    <dc:date>2023-09-19T13:40:39Z</dc:date>
    <item>
      <title>Port AD output on S9S12G</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Port-AD-output-on-S9S12G/m-p/1725555#M19458</link>
      <description>&lt;P&gt;Hi, I am having a problem with an S9S12G96, I have to use the AD port as output. On CODEWARRIOR Processor Expert correctly initializes the port:&lt;BR /&gt;MOVB #255,DDR0AD&lt;BR /&gt;MOVB #255,DDR1AD&lt;BR /&gt;I make it clear that I do not use these ports for anything else (ADC...)&lt;BR /&gt;The ADH and ADL ports seem to be configured as output, but I cannot control them... the lines:&lt;BR /&gt;MOVB #255, PT1AD&lt;BR /&gt;MOVB #255, PT0AD&lt;BR /&gt;Seem inoperable, outputs remain at 0&lt;BR /&gt;Someone ? to help me ?&lt;BR /&gt;THANKS !!!&lt;/P&gt;</description>
      <pubDate>Tue, 19 Sep 2023 13:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Port-AD-output-on-S9S12G/m-p/1725555#M19458</guid>
      <dc:creator>Didier91</dc:creator>
      <dc:date>2023-09-19T13:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: Port AD output on S9S12G</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Port-AD-output-on-S9S12G/m-p/1728596#M19468</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose external circuits connected to the AD do not influence output value at the pin.&lt;/P&gt;
&lt;P&gt;Do you measure a correct port PT1AD registers sets pins PAD0-PAD7 of the MCU?&lt;/P&gt;
&lt;P&gt;Have you tested it out of PE tool?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 06:48:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Port-AD-output-on-S9S12G/m-p/1728596#M19468</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2023-09-25T06:48:05Z</dc:date>
    </item>
    <item>
      <title>Re: Port AD output on S9S12G</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Port-AD-output-on-S9S12G/m-p/1729006#M19469</link>
      <description>&lt;P&gt;Thnk you for your reply ...&lt;/P&gt;&lt;P&gt;With over 40 years of experience, fortunately I don't make such mistakes.&lt;/P&gt;&lt;P&gt;However I found the anomaly on a forum:&lt;BR /&gt;Just run these 2 lines of code:&lt;BR /&gt;MOVB #255, ATDDIENL&lt;BR /&gt;MOVB #255, ATDDIENH&lt;BR /&gt;While the ADC device is disabled!!!!&lt;BR /&gt;Good day&lt;BR /&gt;Didier&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 14:24:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Port-AD-output-on-S9S12G/m-p/1729006#M19469</guid>
      <dc:creator>Didier91</dc:creator>
      <dc:date>2023-09-25T14:24:39Z</dc:date>
    </item>
  </channel>
</rss>