<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: GDU DC link wrong measurement</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-DC-link-wrong-measurement/m-p/1660581#M19205</link>
    <description>&lt;P&gt;Hi lama,&lt;/P&gt;&lt;P&gt;thank you for your reply.&lt;/P&gt;&lt;P&gt;I have checked and everything seems fine. But anyway, if there was something wrong as you said, I would have errors in any ADC conversion, but in my case only the battery voltage coming from the GDU DC Link has this mismatch.&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
    <pubDate>Wed, 31 May 2023 08:03:20 GMT</pubDate>
    <dc:creator>buch2001</dc:creator>
    <dc:date>2023-05-31T08:03:20Z</dc:date>
    <item>
      <title>GDU DC link wrong measurement</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-DC-link-wrong-measurement/m-p/1659631#M19198</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I inherited a project and, trying to solve some problems, I found this behavior that I can't explain.&lt;/P&gt;&lt;P&gt;We use the internal channel 3: GDU DC link to measure the supply voltage, but the measurement is always higher than expected.&lt;/P&gt;&lt;P&gt;For example: I measure with the multimeter on the GHD pin 12.5V but the ADC always returns 520bits, which corresponds to 520*5/1024*5=12.69V (bits*full_range/max_bit*divider)&lt;/P&gt;&lt;P&gt;I know that the result is compliant with the divider tolerance (4.9/5.1), but the error is systematic and I have tried different boards and so I don't think is a divider problem..&lt;/P&gt;&lt;P&gt;Is there something I am missing?&lt;/P&gt;&lt;P&gt;Any help is greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
      <pubDate>Tue, 30 May 2023 13:28:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-DC-link-wrong-measurement/m-p/1659631#M19198</guid>
      <dc:creator>buch2001</dc:creator>
      <dc:date>2023-05-30T13:28:14Z</dc:date>
    </item>
    <item>
      <title>Re: GDU DC link wrong measurement</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-DC-link-wrong-measurement/m-p/1660514#M19202</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I would like to share what came into my mind....&lt;/P&gt;
&lt;P&gt;incorrect vrh, vrl (vrhsel, vrlsel) + used/unused external PNP which defines reference (Ref. manual Chapter B.1 VREG Electrical Specifications itm 4a,4b, 4c)&lt;BR /&gt;incorrect atd clock&lt;BR /&gt;not solved unused ATD pins (from AN4867.pdf: ADC unused pins should be grounded to reduce leakage currents.)&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 07:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-DC-link-wrong-measurement/m-p/1660514#M19202</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2023-05-31T07:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: GDU DC link wrong measurement</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-DC-link-wrong-measurement/m-p/1660581#M19205</link>
      <description>&lt;P&gt;Hi lama,&lt;/P&gt;&lt;P&gt;thank you for your reply.&lt;/P&gt;&lt;P&gt;I have checked and everything seems fine. But anyway, if there was something wrong as you said, I would have errors in any ADC conversion, but in my case only the battery voltage coming from the GDU DC Link has this mismatch.&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 08:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/GDU-DC-link-wrong-measurement/m-p/1660581#M19205</guid>
      <dc:creator>buch2001</dc:creator>
      <dc:date>2023-05-31T08:03:20Z</dc:date>
    </item>
  </channel>
</rss>