<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Rise time for PP7 pin in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rise-time-for-PP7-pin/m-p/1627718#M19145</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Yes.&lt;/P&gt;
&lt;P&gt;However, one mistake....&amp;nbsp; 8ns not 8us..it was a typo. 8us would be absolutely unacceptable.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
    <pubDate>Tue, 04 Apr 2023 13:51:00 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2023-04-04T13:51:00Z</dc:date>
    <item>
      <title>Rise time for PP7 pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rise-time-for-PP7-pin/m-p/1626562#M19141</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on an application using S912ZVL CPU and a hall sensor. We want to supply the hall sensor from PP7 (used as a switched Vdd).&lt;/P&gt;&lt;P&gt;The hall sensor has a&amp;nbsp;Power Up ramp time of 10us. What is the riser time of PP7? Can 10us be achieved?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 05:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rise-time-for-PP7-pin/m-p/1626562#M19141</guid>
      <dc:creator>silviurn</dc:creator>
      <dc:date>2023-04-03T05:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: Rise time for PP7 pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rise-time-for-PP7-pin/m-p/1626781#M19142</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We are really sorry but there was never this data a part of the data sheet in S12(X)+Magni V family devices.&lt;BR /&gt;I have also checked communication related to this topic from application groups and all of them claim that nothing like this was published and also no ibis model was published.&lt;BR /&gt;The only way I would use to provide an answer is that all pins are the same but only some of them have higher drive capability. The value for rise/fall time can be derived from the value mentioned for SPI module where the max value is 8us without load.&lt;BR /&gt;I am very sorry for info I am able to provide but there is really nothing published.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 09:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rise-time-for-PP7-pin/m-p/1626781#M19142</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2023-04-03T09:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: Rise time for PP7 pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rise-time-for-PP7-pin/m-p/1626789#M19143</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="silviurn_0-1680516455741.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/217506i0B091CBC1320658E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="silviurn_0-1680516455741.png" alt="silviurn_0-1680516455741.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;silviurn_0-1680516455741.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you, Ladislav for your quick resolution. I have 1 question:&lt;/P&gt;&lt;P&gt;Rise time and fall time is 8ns like in datasheet or 8us as you stated above?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 10:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rise-time-for-PP7-pin/m-p/1626789#M19143</guid>
      <dc:creator>silviurn</dc:creator>
      <dc:date>2023-04-03T10:09:12Z</dc:date>
    </item>
    <item>
      <title>Re: Rise time for PP7 pin</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rise-time-for-PP7-pin/m-p/1627718#M19145</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Yes.&lt;/P&gt;
&lt;P&gt;However, one mistake....&amp;nbsp; 8ns not 8us..it was a typo. 8us would be absolutely unacceptable.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 13:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Rise-time-for-PP7-pin/m-p/1627718#M19145</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2023-04-04T13:51:00Z</dc:date>
    </item>
  </channel>
</rss>