<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Multiple LIN slave handling and NPF issue in codewarrior while adding new node</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Multiple-LIN-slave-handling-and-NPF-issue-in-codewarrior-while/m-p/1619722#M19138</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am Using MCU - MC9S12ZVML128 and i want to implement single master and 2 slaves in LIN communication. I have already implemented single master and single slave already it is working fine.&lt;/P&gt;&lt;P&gt;Question 1:&lt;/P&gt;&lt;P&gt;I am trying to add another network in LIN network in NPF codewarrior. but it is not allowing me to add due to same timer channel and i cannot change timer channel function because it is disabled in codewarrior.&lt;/P&gt;&lt;P&gt;how can I add new network or enable in timer channel in NPF codewarrior.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dhruvish1_0-1679481324993.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/215760i7A5982D3468C8D4F/image-size/medium?v=v2&amp;amp;px=400" alt="dhruvish1_0-1679481324993.png" title="dhruvish1_0-1679481324993.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question 2 :&amp;nbsp;&lt;/P&gt;&lt;P&gt;if i have to handle multiple slaves what changes i have to make in LIN firmware and how can I handle multiple slaves at same time to get data?&lt;/P&gt;</description>
    <pubDate>Wed, 22 Mar 2023 10:37:39 GMT</pubDate>
    <dc:creator>dhruvish1</dc:creator>
    <dc:date>2023-03-22T10:37:39Z</dc:date>
    <item>
      <title>Multiple LIN slave handling and NPF issue in codewarrior while adding new node</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Multiple-LIN-slave-handling-and-NPF-issue-in-codewarrior-while/m-p/1619722#M19138</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am Using MCU - MC9S12ZVML128 and i want to implement single master and 2 slaves in LIN communication. I have already implemented single master and single slave already it is working fine.&lt;/P&gt;&lt;P&gt;Question 1:&lt;/P&gt;&lt;P&gt;I am trying to add another network in LIN network in NPF codewarrior. but it is not allowing me to add due to same timer channel and i cannot change timer channel function because it is disabled in codewarrior.&lt;/P&gt;&lt;P&gt;how can I add new network or enable in timer channel in NPF codewarrior.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dhruvish1_0-1679481324993.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/215760i7A5982D3468C8D4F/image-size/medium?v=v2&amp;amp;px=400" alt="dhruvish1_0-1679481324993.png" title="dhruvish1_0-1679481324993.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question 2 :&amp;nbsp;&lt;/P&gt;&lt;P&gt;if i have to handle multiple slaves what changes i have to make in LIN firmware and how can I handle multiple slaves at same time to get data?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Mar 2023 10:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Multiple-LIN-slave-handling-and-NPF-issue-in-codewarrior-while/m-p/1619722#M19138</guid>
      <dc:creator>dhruvish1</dc:creator>
      <dc:date>2023-03-22T10:37:39Z</dc:date>
    </item>
  </channel>
</rss>