<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックS912zvml64 How to add LIN communication code separately</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912zvml64-How-to-add-LIN-communication-code-separately/m-p/1591093#M19063</link>
    <description>&lt;P&gt;&lt;STRONG&gt;I am using s912zvml64 as the motor driver, but there is no LIN communication module in the motor code, so I can't realize LIN communication with the outside. So how can I add LIN communication code separately in s912zvml64? Is there any reference routine? Thank you.&lt;/STRONG&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Feb 2023 07:50:09 GMT</pubDate>
    <dc:creator>mine233</dc:creator>
    <dc:date>2023-02-01T07:50:09Z</dc:date>
    <item>
      <title>S912zvml64 How to add LIN communication code separately</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912zvml64-How-to-add-LIN-communication-code-separately/m-p/1591093#M19063</link>
      <description>&lt;P&gt;&lt;STRONG&gt;I am using s912zvml64 as the motor driver, but there is no LIN communication module in the motor code, so I can't realize LIN communication with the outside. So how can I add LIN communication code separately in s912zvml64? Is there any reference routine? Thank you.&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 07:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912zvml64-How-to-add-LIN-communication-code-separately/m-p/1591093#M19063</guid>
      <dc:creator>mine233</dc:creator>
      <dc:date>2023-02-01T07:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: S912zvml64 How to add LIN communication code separately</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912zvml64-How-to-add-LIN-communication-code-separately/m-p/1591548#M19065</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;If you use our SW files for motor control then we do not modify them. They ar AS IS without modification support.&lt;/P&gt;
&lt;P&gt;Please, look at the application note AN5122 Using NXP’s LIN Driver with the MagniV Family&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5122.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5122.pdf&lt;/A&gt; &lt;BR /&gt;The link to the SW you can find here:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/List-of-MagniV-and-S12-X-Application-notes/ta-p/1120728https://community.nxp.com/t5/S12-MagniV-Microcontrollers/List-of-MagniV-and-S12-X-Application-notes/ta-p/1120728" target="_blank"&gt;https://community.nxp.com/t5/S12-MagniV-Microcontrollers/List-of-MagniV-and-S12-X-Application-notes/ta-p/1120728https://community.nxp.com/t5/S12-MagniV-Microcontrollers/List-of-MagniV-and-S12-X-Application-notes/ta-p/1120728&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The LIN2.x and SAE J2602 Stack can be found in the part BSP, Drivers and Middleware at the page&lt;BR /&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-magniv-mixed-signal-mcus/s12zvm-mixed-signal-mcu-for-automotive-industrial-motor-control-applications:S12ZVM" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-magniv-mixed-signal-mcus/s12zvm-mixed-signal-mcu-for-automotive-industrial-motor-control-applications:S12ZVM&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Probably the issue can be that there can be a collision in used timers so this should be considered in application.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 19:30:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S912zvml64-How-to-add-LIN-communication-code-separately/m-p/1591548#M19065</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2023-02-01T19:30:01Z</dc:date>
    </item>
  </channel>
</rss>