<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s12zvml31  Motor driver transplant in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/s12zvml31-Motor-driver-transplant/m-p/1523433#M18846</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I hope this AN will help you...&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5330.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5330.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
    <pubDate>Fri, 16 Sep 2022 06:47:54 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2022-09-16T06:47:54Z</dc:date>
    <item>
      <title>s12zvml31  Motor driver transplant</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/s12zvml31-Motor-driver-transplant/m-p/1522532#M18845</link>
      <description>&lt;P&gt;I want to transplant the motor driver program based on s12zvml128 to s12zvml31. The modified program can be burned to the development board of s12zvml31, but the motor cannot run, and the program transplanted to s12zvml31 cannot enter the ADC interrupt, so the foc algorithm cannot be performed. Do the ADC, timer, and interrupt of s12zvml128 and s12zvml31 need to be configured accordingly?&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 05:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/s12zvml31-Motor-driver-transplant/m-p/1522532#M18845</guid>
      <dc:creator>mine233</dc:creator>
      <dc:date>2022-09-15T05:07:20Z</dc:date>
    </item>
    <item>
      <title>Re: s12zvml31  Motor driver transplant</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/s12zvml31-Motor-driver-transplant/m-p/1523433#M18846</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I hope this AN will help you...&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5330.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5330.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Fri, 16 Sep 2022 06:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/s12zvml31-Motor-driver-transplant/m-p/1523433#M18846</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2022-09-16T06:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: s12zvml31  Motor driver transplant</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/s12zvml31-Motor-driver-transplant/m-p/1523900#M18850</link>
      <description>&lt;P&gt;According to the modification of this document, the program can now run normally on s12zvml31, but the oil pump motor still cannot work normally. Do you need to send external signals through freemaster software to drive the motor?&lt;/P&gt;</description>
      <pubDate>Mon, 19 Sep 2022 01:26:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/s12zvml31-Motor-driver-transplant/m-p/1523900#M18850</guid>
      <dc:creator>mine233</dc:creator>
      <dc:date>2022-09-19T01:26:38Z</dc:date>
    </item>
  </channel>
</rss>