<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックCAN sample point selection in zvml64 mcu</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-sample-point-selection-in-zvml64-mcu/m-p/1503787#M18774</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S12ZVML64 MCU.&lt;/P&gt;&lt;P&gt;For Can Baudrate of 500Kbps&lt;/P&gt;&lt;P&gt;i am checking on two different bus clock&lt;/P&gt;&lt;P&gt;1) With bus clock of 25MHz as&amp;nbsp;CAN source clock&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Time Segment 1 = 16Tq&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Time segment 2 = 8Tq&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Prescaler value = 2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SYNC_SEG = 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sampling Point(%) as calculated is 68%&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2) With bus clock of 20MHz as CAN source clock&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Time Segment 1 = 12Tq&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Time segment 2 = 7Tq&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Prescaler value = 2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SYNC_SEG = 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sampling Point(%) as calculated is 65%&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;So I want to ask what are the parameter on which sample point &lt;SPAN&gt;(%)&amp;nbsp;&lt;/SPAN&gt;selection is decided and is it possible to achieve the same sample point percentage for different frequency i.e 20Mhz and 25Mhz&lt;/P&gt;&lt;P&gt;what is the deciding factor for selection&lt;SPAN&gt;&amp;nbsp;of sampling point for the s12zvml64 MCU.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 10 Aug 2022 07:54:35 GMT</pubDate>
    <dc:creator>pratayay123</dc:creator>
    <dc:date>2022-08-10T07:54:35Z</dc:date>
    <item>
      <title>CAN sample point selection in zvml64 mcu</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-sample-point-selection-in-zvml64-mcu/m-p/1503787#M18774</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S12ZVML64 MCU.&lt;/P&gt;&lt;P&gt;For Can Baudrate of 500Kbps&lt;/P&gt;&lt;P&gt;i am checking on two different bus clock&lt;/P&gt;&lt;P&gt;1) With bus clock of 25MHz as&amp;nbsp;CAN source clock&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Time Segment 1 = 16Tq&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Time segment 2 = 8Tq&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Prescaler value = 2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SYNC_SEG = 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sampling Point(%) as calculated is 68%&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2) With bus clock of 20MHz as CAN source clock&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Time Segment 1 = 12Tq&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Time segment 2 = 7Tq&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Prescaler value = 2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SYNC_SEG = 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sampling Point(%) as calculated is 65%&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;So I want to ask what are the parameter on which sample point &lt;SPAN&gt;(%)&amp;nbsp;&lt;/SPAN&gt;selection is decided and is it possible to achieve the same sample point percentage for different frequency i.e 20Mhz and 25Mhz&lt;/P&gt;&lt;P&gt;what is the deciding factor for selection&lt;SPAN&gt;&amp;nbsp;of sampling point for the s12zvml64 MCU.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 07:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-sample-point-selection-in-zvml64-mcu/m-p/1503787#M18774</guid>
      <dc:creator>pratayay123</dc:creator>
      <dc:date>2022-08-10T07:54:35Z</dc:date>
    </item>
    <item>
      <title>Re: CAN sample point selection in zvml64 mcu</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-sample-point-selection-in-zvml64-mcu/m-p/1505471#M18776</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;sampling point is up to the user or some specification.&lt;/P&gt;
&lt;P&gt;A good general rule is to set the sample point above 80%. Based on the experiences of the automotive industry, the selected sample point should be near the 80% value.&lt;/P&gt;
&lt;P&gt;To play a small game you can use &lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-setup-calculator-for-S12-X-and-MagniV-devices/ta-p/1111309" target="_blank"&gt;https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-setup-calculator-for-S12-X-and-MagniV-devices/ta-p/1111309&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;where all combinations are calculated and suitable ones are highlighted.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN1798.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN1798.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Fri, 12 Aug 2022 08:18:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-sample-point-selection-in-zvml64-mcu/m-p/1505471#M18776</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2022-08-12T08:18:27Z</dc:date>
    </item>
  </channel>
</rss>