<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCS9S12G STOP mode current in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MCS9S12G-STOP-mode-current/m-p/1497744#M18755</link>
    <description>&lt;P&gt;When I use this chip, after entering the STOP mode, the current consumption is 2mA, and the unused IO ports have also entered the pull-up input mode. Is there any way to reduce power consumption?&lt;/P&gt;</description>
    <pubDate>Fri, 29 Jul 2022 05:21:41 GMT</pubDate>
    <dc:creator>wenfengyao</dc:creator>
    <dc:date>2022-07-29T05:21:41Z</dc:date>
    <item>
      <title>MCS9S12G STOP mode current</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MCS9S12G-STOP-mode-current/m-p/1497744#M18755</link>
      <description>&lt;P&gt;When I use this chip, after entering the STOP mode, the current consumption is 2mA, and the unused IO ports have also entered the pull-up input mode. Is there any way to reduce power consumption?&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jul 2022 05:21:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MCS9S12G-STOP-mode-current/m-p/1497744#M18755</guid>
      <dc:creator>wenfengyao</dc:creator>
      <dc:date>2022-07-29T05:21:41Z</dc:date>
    </item>
    <item>
      <title>Re: MCS9S12G STOP mode current</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MCS9S12G-STOP-mode-current/m-p/1499271#M18757</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The device is CMOS technology device so in full stop mode there is no reason for an additional current. Except, if there are some „sources“/grounds connected via pins to ground/„sources“. In this case you have to think how to avoid this additional consumption ( for example; lighting diode either switched to gnd or Vdd, sensor, input of another device)&lt;BR /&gt;The question is also where you measure the consumption.&lt;BR /&gt;Is your mode full stop .... is everything switched off? (Pseudo stop mode)&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 06:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MCS9S12G-STOP-mode-current/m-p/1499271#M18757</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2022-08-02T06:19:23Z</dc:date>
    </item>
  </channel>
</rss>