<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: bootloader mc9s12xeg128</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1461901#M18670</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I created the interrupt vector table with processor export and was able to set up the serial port. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I also did not need to create a code in the RAM section and replaced the following phrase&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;// # pragma CODE_SEG RAM_CODE &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;#pragma CODE_SEG NON_BANKED&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 21 May 2022 05:33:05 GMT</pubDate>
    <dc:creator>javadshabani</dc:creator>
    <dc:date>2022-05-21T05:33:05Z</dc:date>
    <item>
      <title>bootloader mc9s12xeg128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1451699#M18632</link>
      <description>&lt;P&gt;hello every one&lt;/P&gt;&lt;P&gt;i am working on mc9s12xeg128MAL (or mc9s12xet256mal) for writing a bootloader. i am download the&amp;nbsp;AN4258SW and use&amp;nbsp;Bootloader_S12X example, but it seems this code is hanging.&lt;/P&gt;&lt;P&gt;i have multilink universal fx for debuging.&lt;/P&gt;</description>
      <pubDate>Mon, 02 May 2022 07:04:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1451699#M18632</guid>
      <dc:creator>javadshabani</dc:creator>
      <dc:date>2022-05-02T07:04:08Z</dc:date>
    </item>
    <item>
      <title>Re: bootloader mc9s12xeg128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1451701#M18633</link>
      <description>&lt;PRE&gt;I have read the documents required for bootloader, but I have trouble setting it up&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 May 2022 07:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1451701#M18633</guid>
      <dc:creator>javadshabani</dc:creator>
      <dc:date>2022-05-02T07:09:47Z</dc:date>
    </item>
    <item>
      <title>Re: bootloader mc9s12xeg128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1454529#M18645</link>
      <description>&lt;P&gt;i am used the&amp;nbsp;AN4258SW&amp;nbsp; sample code but When the interrupt is activated and the interrupt occurs, the program hangs.&lt;/P&gt;&lt;P&gt;i am send serial data when interrupt disabled, after send 0x55 two time, interrupt enabled and program hangs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 08 May 2022 05:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1454529#M18645</guid>
      <dc:creator>javadshabani</dc:creator>
      <dc:date>2022-05-08T05:03:02Z</dc:date>
    </item>
    <item>
      <title>Re: bootloader mc9s12xeg128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1460964#M18668</link>
      <description>&lt;P&gt;Hi Javad,&lt;/P&gt;
&lt;P&gt;I can see in the code that you commented out function CopyCodeToRAM(). However, the interrupt handlers are placed to RAM, so this won't work. Interrupt is triggered but there's no valid handler in this case.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 19 May 2022 14:04:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1460964#M18668</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-05-19T14:04:49Z</dc:date>
    </item>
    <item>
      <title>Re: bootloader mc9s12xeg128</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1461901#M18670</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I created the interrupt vector table with processor export and was able to set up the serial port. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I also did not need to create a code in the RAM section and replaced the following phrase&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;// # pragma CODE_SEG RAM_CODE &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;#pragma CODE_SEG NON_BANKED&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 21 May 2022 05:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/bootloader-mc9s12xeg128/m-p/1461901#M18670</guid>
      <dc:creator>javadshabani</dc:creator>
      <dc:date>2022-05-21T05:33:05Z</dc:date>
    </item>
  </channel>
</rss>