<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Bootloader timer interrupt</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-timer-interrupt/m-p/1413039#M18497</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;As given in the link only we are going to create project ,&lt;/P&gt;&lt;P&gt;need some answer to the below queries :&lt;/P&gt;&lt;P&gt;1) For Bootloader project we need timer interrupt to be implemented and user application also uses many&amp;nbsp; type of interrupt can we merge these projects.&lt;/P&gt;&lt;P&gt;2) For Bootloader we require to implement a separate timer interrupt how it can be done can you please share some sample code for the same.&lt;/P&gt;</description>
    <pubDate>Mon, 14 Feb 2022 10:38:33 GMT</pubDate>
    <dc:creator>pratibhasurabhi</dc:creator>
    <dc:date>2022-02-14T10:38:33Z</dc:date>
    <item>
      <title>Bootloader timer interrupt</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-timer-interrupt/m-p/1411528#M18488</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using s12zvml64 series mcu with code warrior 10.7&lt;/P&gt;&lt;P&gt;I am creating a bootloader project , m&lt;SPAN&gt;y project contains both user application and bootloader.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;As with current scenario interrupt is&amp;nbsp;getting&amp;nbsp;hit in application code area and from there i am calling an ISR function to be executed that is defined in bootloader area so while hitting the interrupt the code is not going to the ISR functionality&amp;nbsp;, as interrupt vector is defined in application code area and when the code is coming to bootloader area it is clearing the application code area.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So what can we do to access the timer interrupt in bootloader.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am looking forward to the reply,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Feb 2022 04:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-timer-interrupt/m-p/1411528#M18488</guid>
      <dc:creator>pratibhasurabhi</dc:creator>
      <dc:date>2022-02-10T04:37:15Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader timer interrupt</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-timer-interrupt/m-p/1412952#M18496</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The approach you do is really not recommended. A bootloader and the application should be created as two absolutely independent applications to ensure all possible overlapping problems and to avoid any possible incorrect addressing, jump or return.&lt;/P&gt;
&lt;P&gt;To know something about good approach I suggest to read&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Simple-Serial-Bootloader-for-S12Z-AN-draft/ta-p/1126452" target="_blank"&gt;https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Simple-Serial-Bootloader-for-S12Z-AN-draft/ta-p/1126452&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 14 Feb 2022 08:11:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-timer-interrupt/m-p/1412952#M18496</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2022-02-14T08:11:30Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader timer interrupt</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-timer-interrupt/m-p/1413039#M18497</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;As given in the link only we are going to create project ,&lt;/P&gt;&lt;P&gt;need some answer to the below queries :&lt;/P&gt;&lt;P&gt;1) For Bootloader project we need timer interrupt to be implemented and user application also uses many&amp;nbsp; type of interrupt can we merge these projects.&lt;/P&gt;&lt;P&gt;2) For Bootloader we require to implement a separate timer interrupt how it can be done can you please share some sample code for the same.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Feb 2022 10:38:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-timer-interrupt/m-p/1413039#M18497</guid>
      <dc:creator>pratibhasurabhi</dc:creator>
      <dc:date>2022-02-14T10:38:33Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader timer interrupt</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-timer-interrupt/m-p/1413911#M18504</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;2) S12Z are equipped with IVBR register, which allows both, bootloader and application to have their own interrupt vector tables and their own ISRs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) You can't easily merge application with bootloader in the same project. It is possible but error prone. It is easier to include compiled bootloader code in application project, so that you can easily build production image of app+bootloader or debug with both app and bootloader programmed to flash memory.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;</description>
      <pubDate>Tue, 15 Feb 2022 21:28:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-timer-interrupt/m-p/1413911#M18504</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2022-02-15T21:28:09Z</dc:date>
    </item>
  </channel>
</rss>