<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: MM9Z1_638 CAN receiver error</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-CAN-receiver-error/m-p/1402563#M18421</link>
    <description>&lt;P&gt;I am working with CAN transmission on MM9Z1_638 with demo board RD9Z1_638_4Li Rev 1.2, We establish CAN communication between MM9Z1_638 and MICROCHIP CAN analyzer with demo code (RD9Z1_638_12VLA_CAN_demo). The data is transmitting from MM9Z1_638 to CAN analyzer is ok and receiving data from CAN analyzer to MM9Z1_638 is also working fine. But while working on power saving modes , i observed the below commands for sleep mode(CAN_IBS_Control.u16Var&amp;amp;0x8000), calibration mode(CAN_IBS_Control.u16Var&amp;amp;0x1000) &amp;amp; normal mode(CAN_IBS_Control.u16Var&amp;amp;0x2000) commands and Please help me to understanding these commands.&lt;/P&gt;&lt;P&gt;Here i am attching the code&amp;nbsp;&lt;/P&gt;&lt;P&gt;// read message object .....&lt;BR /&gt;(void) Check_CAN_MB_Status(CAN0, CANBUF3, &amp;amp;mbStat);&lt;BR /&gt;if((mbStat.Status == NEWDATA) || (mbStat.Status == OVERRUN)) { //Wait for the Receive ISR to finish and change the buffer status, NEWDATA indicates that the buffer has receive a new data&lt;BR /&gt;&lt;BR /&gt;err_status = Read_CAN_MB_Data(CAN0, CANBUF3, CAN_IBS_Control.byte);//Copy the received data in msCAN channel 0 buffer 2 to data_rec;&lt;BR /&gt;CAN_IBS_Control.u16Var = u16Swap(CAN_IBS_Control.u16Var);&lt;BR /&gt;//Clear buffer_status[0]&lt;BR /&gt;//err_status = Read_CAN_MB_Data(CAN0, CANBUF3, rec_data);&lt;BR /&gt;err_status = Load_CAN_MB(CAN0, CANBUF1, CAN_IBS_Control.byte);&lt;BR /&gt;err_status = Transmit_CAN_MB(CAN0, CANBUF1);&lt;BR /&gt;mbStat.Status = NODATA;&lt;BR /&gt;&lt;BR /&gt;if(CAN_IBS_Control.u16Var&amp;amp;0x8000) { // Goto Sleep Request&lt;BR /&gt;// goto sleep&lt;BR /&gt;err_status = Sleep_CAN(CAN0, CMPTX); // request CAN channel 0 go to sleep with completing transmission scheduled&lt;BR /&gt;do {&lt;BR /&gt;err_status = Check_CAN_Status(CAN0,CAN_status); // read the channel 0 status&lt;BR /&gt;}while (!(CAN_status[1]&amp;amp;SLPAK)); // wait till SLPAK bit set&lt;/P&gt;&lt;P&gt;//B_PCR_WUEH_WUPTB4 = 1; // enable PTB4 wakeup&lt;BR /&gt;ADCDisable();&lt;BR /&gt;TsenseDisable();&lt;BR /&gt;B_GPIO_VSENSE = 0;&lt;/P&gt;&lt;P&gt;CAN_STDBY(STANDBYMODE);&lt;BR /&gt;PTA_PTA1 = 0;&lt;BR /&gt;PCREnterStopMode();&lt;/P&gt;&lt;P&gt;// .....zzzzzzzzzzz (stop mode)&lt;BR /&gt;// after wakeup the code continues to run here....&lt;BR /&gt;// but first the D2D Interrupt service routine will be run&lt;BR /&gt;B_WD_CTL = WD_OFF;&lt;BR /&gt;VsenseInit(&amp;amp;(vList[0]), &amp;amp;vListEntries, &amp;amp;(vValues[0]));&lt;BR /&gt;CsenseInit(&amp;amp;(cList[0]), &amp;amp;cListEntries, &amp;amp;(cValues[0]));&lt;BR /&gt;TsenseInit(&amp;amp;(tList[0]), &amp;amp;tListEntries, &amp;amp;(tValues[0]));&lt;BR /&gt;ADCInit();&lt;BR /&gt;CAN_STDBY(NORMALMODE);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;if(CAN_IBS_Control.u16Var&amp;amp;0x1000) { // Goto Calib mode&lt;BR /&gt;Battery.tMode = BM_CALIBRATION;&lt;/P&gt;&lt;P&gt;CAN_IBS_Data.BatMode = Battery.tMode;&lt;BR /&gt;err_status = Load_CAN_MB(CAN0, CANBUF1, CAN_IBS_Data.byte);&lt;BR /&gt;err_status = Transmit_CAN_MB(CAN0, CANBUF1);&lt;BR /&gt;&lt;BR /&gt;err_status = Config_CAN_MB (CAN0, 8, RXDF, 8);&lt;BR /&gt;err_status = Config_CAN_MB (CAN0, 9, TXDF, 9);&lt;BR /&gt;}&lt;BR /&gt;if(CAN_IBS_Control.u16Var&amp;amp;0x2000) { // Goto normal mode&lt;BR /&gt;Battery.tMode = BM_DRIVING;&lt;BR /&gt;VsenseInit(&amp;amp;(vList[0]), &amp;amp;vListEntries, &amp;amp;(vValues[0]));&lt;BR /&gt;CsenseInit(&amp;amp;(cList[0]), &amp;amp;cListEntries, &amp;amp;(cValues[0]));&lt;BR /&gt;TsenseInit(&amp;amp;(tList[0]), &amp;amp;tListEntries, &amp;amp;(tValues[0]));&lt;BR /&gt;ADCInit();&lt;BR /&gt;}&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jan 2022 10:20:12 GMT</pubDate>
    <dc:creator>baji</dc:creator>
    <dc:date>2022-01-20T10:20:12Z</dc:date>
    <item>
      <title>MM9Z1_638 CAN receiver error</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-CAN-receiver-error/m-p/1394734#M18373</link>
      <description>&lt;P&gt;&lt;SPAN&gt;We are working with CAN transmission on MM9Z1_638 with demo board RD9Z1_638_4Li Rev 1.2, We establish CAN communication between MM9Z1_638 and MICROCHIP CAN analyzer with demo code (RD9Z1_638_12VLA_CAN_demo). The data is transmitting from MM9Z1_638 to CAN analyzer is ok and receiving data from CAN analyzer to MM9Z1_638 is not getting and it is showing OVERRUN problem. Please help me to sort of this error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Here i am attching the receiving code in demo code&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;// read message object .....&lt;BR /&gt;(void) Check_CAN_MB_Status(CAN0, CANBUF3, &amp;amp;mbStat);&lt;BR /&gt;if(mbStat.Status == NEWDATA)&lt;BR /&gt;{ //Wait for the Receive ISR to finish and change the buffer status, NEWDATA indicates that the buffer has receive a new data&lt;BR /&gt;&lt;BR /&gt;err_status = Read_CAN_MB_Data(CAN0, CANBUF3, CAN_IBS_Control.byte);//Copy the received data in msCAN channel 0 buffer 2 to data_rec;&lt;BR /&gt;CAN_IBS_Control.u16Var = u16Swap(CAN_IBS_Control.u16Var);&lt;BR /&gt;mbStat.Status = NODATA; //Clear buffer_status[0]&lt;BR /&gt;//err_status = Read_CAN_MB_Data(CAN0, CANBUF3, rec_data);&lt;BR /&gt;&lt;BR /&gt;if(CAN_IBS_Control.u16Var&amp;amp;0x8000) { // Goto Sleep Request&lt;BR /&gt;// goto sleep&lt;BR /&gt;err_status = Sleep_CAN(CAN0, CMPTX); // request CAN channel 0 go to sleep with completing transmission scheduled&lt;/P&gt;&lt;P&gt;do {&lt;BR /&gt;err_status = Check_CAN_Status(CAN0,CAN_status); // read the channel 0 status&lt;BR /&gt;}while (!(CAN_status[1]&amp;amp;SLPAK)); // wait till SLPAK bit set&lt;/P&gt;&lt;P&gt;B_PCR_WUEH_WUPTB4 = 1; // enable PTB4 wakeup&lt;BR /&gt;ADCDisable();&lt;BR /&gt;TsenseDisable();&lt;BR /&gt;B_GPIO_VSENSE = 0;&lt;/P&gt;&lt;P&gt;CAN_STDBY(STANDBYMODE);&lt;BR /&gt;PTA_PTA1 = 0;&lt;BR /&gt;PCREnterStopMode();&lt;/P&gt;&lt;P&gt;// .....zzzzzzzzzzz (stop mode)&lt;BR /&gt;// after wakeup the code continues to run here....&lt;BR /&gt;// but first the D2D Interrupt service routine will be run&lt;BR /&gt;B_WD_CTL = WD_OFF;&lt;BR /&gt;VsenseInit(&amp;amp;(vList[0]), &amp;amp;vListEntries, &amp;amp;(vValues[0]));&lt;BR /&gt;CsenseInit(&amp;amp;(cList[0]), &amp;amp;cListEntries, &amp;amp;(cValues[0]));&lt;BR /&gt;TsenseInit(&amp;amp;(tList[0]), &amp;amp;tListEntries, &amp;amp;(tValues[0]));&lt;BR /&gt;ADCInit();&lt;BR /&gt;CAN_STDBY(NORMALMODE);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;if(CAN_IBS_Control.u16Var&amp;amp;0x1000) { // Goto Calib mode&lt;BR /&gt;Battery.tMode = BM_CALIBRATION;&lt;/P&gt;&lt;P&gt;CAN_IBS_Data.BatMode = Battery.tMode;&lt;BR /&gt;err_status = Load_CAN_MB(CAN0, CANBUF1, CAN_IBS_Data.byte);&lt;BR /&gt;err_status = Transmit_CAN_MB(CAN0, CANBUF1);&lt;BR /&gt;&lt;BR /&gt;err_status = Config_CAN_MB (CAN0, 8, RXDF, 8);&lt;BR /&gt;err_status = Config_CAN_MB (CAN0, 9, TXDF, 9);&lt;BR /&gt;}&lt;BR /&gt;if(CAN_IBS_Control.u16Var&amp;amp;0x2000) { // Goto normal mode&lt;BR /&gt;Battery.tMode = BM_DRIVING;&lt;BR /&gt;VsenseInit(&amp;amp;(vList[0]), &amp;amp;vListEntries, &amp;amp;(vValues[0]));&lt;BR /&gt;CsenseInit(&amp;amp;(cList[0]), &amp;amp;cListEntries, &amp;amp;(cValues[0]));&lt;BR /&gt;TsenseInit(&amp;amp;(tList[0]), &amp;amp;tListEntries, &amp;amp;(tValues[0]));&lt;BR /&gt;ADCInit();&lt;BR /&gt;}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 09:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-CAN-receiver-error/m-p/1394734#M18373</guid>
      <dc:creator>baji</dc:creator>
      <dc:date>2022-01-05T09:39:09Z</dc:date>
    </item>
    <item>
      <title>Re: MM9Z1_638 CAN receiver error</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-CAN-receiver-error/m-p/1396157#M18381</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186056"&gt;@baji&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm not familiar with the driver and this seems to be an application issue.&lt;/P&gt;
&lt;P&gt;But the OVERRUN probably simply means the CANRFLG_OVRIF gets set.&lt;/P&gt;
&lt;P&gt;Please refer to the datasheet, Section 6.13.4.2.3 Receive structures.&lt;/P&gt;
&lt;P&gt;The code that you posted is polling the status of the can module by calling Check_CAN_MB_Status() in the main endless loop.&lt;/P&gt;
&lt;P&gt;You are probably sending the CAN messages faster than the application can process it.&lt;/P&gt;
&lt;P&gt;Can you send just one message from the CAN bus analyzer and check if it can receive it?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jan 2022 13:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-CAN-receiver-error/m-p/1396157#M18381</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-01-07T13:09:40Z</dc:date>
    </item>
    <item>
      <title>Re: MM9Z1_638 CAN receiver error</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-CAN-receiver-error/m-p/1402563#M18421</link>
      <description>&lt;P&gt;I am working with CAN transmission on MM9Z1_638 with demo board RD9Z1_638_4Li Rev 1.2, We establish CAN communication between MM9Z1_638 and MICROCHIP CAN analyzer with demo code (RD9Z1_638_12VLA_CAN_demo). The data is transmitting from MM9Z1_638 to CAN analyzer is ok and receiving data from CAN analyzer to MM9Z1_638 is also working fine. But while working on power saving modes , i observed the below commands for sleep mode(CAN_IBS_Control.u16Var&amp;amp;0x8000), calibration mode(CAN_IBS_Control.u16Var&amp;amp;0x1000) &amp;amp; normal mode(CAN_IBS_Control.u16Var&amp;amp;0x2000) commands and Please help me to understanding these commands.&lt;/P&gt;&lt;P&gt;Here i am attching the code&amp;nbsp;&lt;/P&gt;&lt;P&gt;// read message object .....&lt;BR /&gt;(void) Check_CAN_MB_Status(CAN0, CANBUF3, &amp;amp;mbStat);&lt;BR /&gt;if((mbStat.Status == NEWDATA) || (mbStat.Status == OVERRUN)) { //Wait for the Receive ISR to finish and change the buffer status, NEWDATA indicates that the buffer has receive a new data&lt;BR /&gt;&lt;BR /&gt;err_status = Read_CAN_MB_Data(CAN0, CANBUF3, CAN_IBS_Control.byte);//Copy the received data in msCAN channel 0 buffer 2 to data_rec;&lt;BR /&gt;CAN_IBS_Control.u16Var = u16Swap(CAN_IBS_Control.u16Var);&lt;BR /&gt;//Clear buffer_status[0]&lt;BR /&gt;//err_status = Read_CAN_MB_Data(CAN0, CANBUF3, rec_data);&lt;BR /&gt;err_status = Load_CAN_MB(CAN0, CANBUF1, CAN_IBS_Control.byte);&lt;BR /&gt;err_status = Transmit_CAN_MB(CAN0, CANBUF1);&lt;BR /&gt;mbStat.Status = NODATA;&lt;BR /&gt;&lt;BR /&gt;if(CAN_IBS_Control.u16Var&amp;amp;0x8000) { // Goto Sleep Request&lt;BR /&gt;// goto sleep&lt;BR /&gt;err_status = Sleep_CAN(CAN0, CMPTX); // request CAN channel 0 go to sleep with completing transmission scheduled&lt;BR /&gt;do {&lt;BR /&gt;err_status = Check_CAN_Status(CAN0,CAN_status); // read the channel 0 status&lt;BR /&gt;}while (!(CAN_status[1]&amp;amp;SLPAK)); // wait till SLPAK bit set&lt;/P&gt;&lt;P&gt;//B_PCR_WUEH_WUPTB4 = 1; // enable PTB4 wakeup&lt;BR /&gt;ADCDisable();&lt;BR /&gt;TsenseDisable();&lt;BR /&gt;B_GPIO_VSENSE = 0;&lt;/P&gt;&lt;P&gt;CAN_STDBY(STANDBYMODE);&lt;BR /&gt;PTA_PTA1 = 0;&lt;BR /&gt;PCREnterStopMode();&lt;/P&gt;&lt;P&gt;// .....zzzzzzzzzzz (stop mode)&lt;BR /&gt;// after wakeup the code continues to run here....&lt;BR /&gt;// but first the D2D Interrupt service routine will be run&lt;BR /&gt;B_WD_CTL = WD_OFF;&lt;BR /&gt;VsenseInit(&amp;amp;(vList[0]), &amp;amp;vListEntries, &amp;amp;(vValues[0]));&lt;BR /&gt;CsenseInit(&amp;amp;(cList[0]), &amp;amp;cListEntries, &amp;amp;(cValues[0]));&lt;BR /&gt;TsenseInit(&amp;amp;(tList[0]), &amp;amp;tListEntries, &amp;amp;(tValues[0]));&lt;BR /&gt;ADCInit();&lt;BR /&gt;CAN_STDBY(NORMALMODE);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;if(CAN_IBS_Control.u16Var&amp;amp;0x1000) { // Goto Calib mode&lt;BR /&gt;Battery.tMode = BM_CALIBRATION;&lt;/P&gt;&lt;P&gt;CAN_IBS_Data.BatMode = Battery.tMode;&lt;BR /&gt;err_status = Load_CAN_MB(CAN0, CANBUF1, CAN_IBS_Data.byte);&lt;BR /&gt;err_status = Transmit_CAN_MB(CAN0, CANBUF1);&lt;BR /&gt;&lt;BR /&gt;err_status = Config_CAN_MB (CAN0, 8, RXDF, 8);&lt;BR /&gt;err_status = Config_CAN_MB (CAN0, 9, TXDF, 9);&lt;BR /&gt;}&lt;BR /&gt;if(CAN_IBS_Control.u16Var&amp;amp;0x2000) { // Goto normal mode&lt;BR /&gt;Battery.tMode = BM_DRIVING;&lt;BR /&gt;VsenseInit(&amp;amp;(vList[0]), &amp;amp;vListEntries, &amp;amp;(vValues[0]));&lt;BR /&gt;CsenseInit(&amp;amp;(cList[0]), &amp;amp;cListEntries, &amp;amp;(cValues[0]));&lt;BR /&gt;TsenseInit(&amp;amp;(tList[0]), &amp;amp;tListEntries, &amp;amp;(tValues[0]));&lt;BR /&gt;ADCInit();&lt;BR /&gt;}&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 10:20:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-CAN-receiver-error/m-p/1402563#M18421</guid>
      <dc:creator>baji</dc:creator>
      <dc:date>2022-01-20T10:20:12Z</dc:date>
    </item>
    <item>
      <title>Re: MM9Z1_638 CAN receiver error</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-CAN-receiver-error/m-p/1403242#M18423</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186056"&gt;@baji&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please see the answer there:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-sleep-mode-issue/td-p/1402560" target="_blank"&gt;https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-sleep-mode-issue/td-p/1402560&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 12:41:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1-638-CAN-receiver-error/m-p/1403242#M18423</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-01-21T12:41:15Z</dc:date>
    </item>
  </channel>
</rss>