<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Bootloader ,Using SRecCvt-GUI to convert S19 file ,No output?? in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-Using-SRecCvt-GUI-to-convert-S19-file-No-output/m-p/1393678#M18362</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I am not able to test it because of your folder structure. However, what I suggest is to copy the original S19 file into the SRecCvt folder and convert it there. It is better to use "no path" access to avoid any problems with tree structure.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
    <pubDate>Mon, 03 Jan 2022 07:13:27 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2022-01-03T07:13:27Z</dc:date>
    <item>
      <title>Bootloader ,Using SRecCvt-GUI to convert S19 file ,No output??</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-Using-SRecCvt-GUI-to-convert-S19-file-No-output/m-p/1393593#M18355</link>
      <description>&lt;P&gt;&lt;STRONG&gt;&lt;SPAN&gt;I just want to use the&amp;nbsp;SRecCvt-GUI to convert the&amp;nbsp;Project.abs.s19 file for CAN-BootLoader(xs128) using.But when I do like the follow&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ChenBowen_0-1641049731937.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166555iEED65274CD201480/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ChenBowen_0-1641049731937.png" alt="ChenBowen_0-1641049731937.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ChenBowen_0-1641049731937.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Why no output?&amp;nbsp; Why the Debug mode says "Can't Open Input File "?&lt;/P&gt;</description>
      <pubDate>Sat, 01 Jan 2022 15:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-Using-SRecCvt-GUI-to-convert-S19-file-No-output/m-p/1393593#M18355</guid>
      <dc:creator>ChenBowen</dc:creator>
      <dc:date>2022-01-01T15:10:43Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader ,Using SRecCvt-GUI to convert S19 file ,No output??</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-Using-SRecCvt-GUI-to-convert-S19-file-No-output/m-p/1393678#M18362</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I am not able to test it because of your folder structure. However, what I suggest is to copy the original S19 file into the SRecCvt folder and convert it there. It is better to use "no path" access to avoid any problems with tree structure.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jan 2022 07:13:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Bootloader-Using-SRecCvt-GUI-to-convert-S19-file-No-output/m-p/1393678#M18362</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2022-01-03T07:13:27Z</dc:date>
    </item>
  </channel>
</rss>