<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: Error while programming mc9s12c32</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133170#M1836</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I had this problem yesterday.&lt;BR /&gt;&lt;BR /&gt;If your code is running when you plug the board in you aren't able to flash it.&amp;nbsp; Therefore in the debug window of CW you need to go into communication-&amp;gt;special tab-&amp;gt;highlight "hot plugging".&amp;nbsp; This fixed my problem.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 May 2007 12:25:53 GMT</pubDate>
    <dc:creator>PhattieM</dc:creator>
    <dc:date>2007-05-10T12:25:53Z</dc:date>
    <item>
      <title>Error while programming mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133166#M1832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I faced a problem while trying to program the mc9s12c32&amp;nbsp; controller .&lt;/DIV&gt;&lt;DIV&gt;The error message i am getting is : Error loading the diagnostic algorithm or incorrect derivative selected.&lt;/DIV&gt;&lt;DIV&gt;I have chosen the HS12 family only.&lt;/DIV&gt;&lt;DIV&gt;I am using Metroworks codewarrior IDE V 3.1 and P&amp;amp; E USB multilink interface for programming.&lt;/DIV&gt;&lt;DIV&gt;Plz help to resolve the issue&lt;/DIV&gt;&lt;DIV&gt;Deepa.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 May 2007 15:40:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133166#M1832</guid>
      <dc:creator>mdeepamenon</dc:creator>
      <dc:date>2007-05-09T15:40:33Z</dc:date>
    </item>
    <item>
      <title>Re: Error while programming mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133167#M1833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;HS12 family does not exist. &lt;BR /&gt;MC9S12C32 is in the choice given by P&amp;amp;E USB Multilink.&lt;BR /&gt;If the device is not selected automatically, you have problems of communication/reset/power of the board.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 May 2007 17:16:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133167#M1833</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-05-09T17:16:22Z</dc:date>
    </item>
    <item>
      <title>Re: Error while programming mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133168#M1834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;sorry , i have selected the correct family.(HC12) Both the set target and set derivative windows automatically detects my target .&lt;/DIV&gt;&lt;DIV&gt;When iam trying to burn the program, the non volatile memory control window appears and displays the above said error message. my program is not burned ultimately.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 May 2007 17:21:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133168#M1834</guid>
      <dc:creator>mdeepamenon</dc:creator>
      <dc:date>2007-05-09T17:21:21Z</dc:date>
    </item>
    <item>
      <title>Re: Error while programming mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133169#M1835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Ok,&lt;BR /&gt;If the device is selected properly automatically, it means your communication between the board and the MCU is proper.&lt;BR /&gt;Try and load an example software and see if you have an error.&lt;BR /&gt;Examples can be found in the CodeWarrior example folder.&lt;BR /&gt;&lt;BR /&gt;If you don't see the error, it is because of the memory areas declared in your personal project.&lt;BR /&gt;If you do see the error, you may have a problem with your microcontroller or the way the debugger/cable are configured.&lt;BR /&gt;&lt;BR /&gt;Cheers.&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 May 2007 17:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133169#M1835</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-05-09T17:39:45Z</dc:date>
    </item>
    <item>
      <title>Re: Error while programming mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133170#M1836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I had this problem yesterday.&lt;BR /&gt;&lt;BR /&gt;If your code is running when you plug the board in you aren't able to flash it.&amp;nbsp; Therefore in the debug window of CW you need to go into communication-&amp;gt;special tab-&amp;gt;highlight "hot plugging".&amp;nbsp; This fixed my problem.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2007 12:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133170#M1836</guid>
      <dc:creator>PhattieM</dc:creator>
      <dc:date>2007-05-10T12:25:53Z</dc:date>
    </item>
    <item>
      <title>Re: Error while programming mc9s12c32</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133171#M1837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;A was solving this problem today morning. The advantage was, that the MCU worked well yesterday and I made some changes on PCB, that I was aware of. I was trying normal single chip mode first and than expanded narrow mode. For the fisrt mode, I had to connect pins MODA and MODB to the ground (log. 0), the second mode needs MODB in log. 0&amp;nbsp; and MODA in log. 1 according to the datasheet. But after taht I changed the pin MODA from log. 0 to log. 1 by hardware pull-up, I haven't be able to burn the program to MCU and I saw the same error message as you wrote. So I disabled the pull-up on MODA and connected it to ground. And the burning worked again and I turned on the expanded narrow mode in processor expert and it works now almost without problems. I have to notice, that I'm using CodeWarrior v 5.7.0 for HCS12 MCUs with free license and Pemicro USB Multilink Rev. C.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 May 2007 18:39:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Error-while-programming-mc9s12c32/m-p/133171#M1837</guid>
      <dc:creator>Tomik</dc:creator>
      <dc:date>2007-05-11T18:39:49Z</dc:date>
    </item>
  </channel>
</rss>