<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: Transferring code from HC9S12DP512 to MC9S12XEP100</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1345225#M18189</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/40626"&gt;@RadekS&lt;/a&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;You got the key point.&lt;BR /&gt;I've set ECT_OCPD_OCPD4 = 0b1 and everything works like a charm now.&lt;BR /&gt;Thanks a lot&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 17:32:30 GMT</pubDate>
    <dc:creator>danielflor</dc:creator>
    <dc:date>2021-09-23T17:32:30Z</dc:date>
    <item>
      <title>Transferring code from HC9S12DP512 to MC9S12XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1342760#M18180</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I'm transferring code from HC9S12DP512 to MC9S12XEP100. But there are some differences that I don't understand, even reading their datasheets.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Here is a code snippet, it is a configuration of a pin of the microcontroller as output compare:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;ECT_TIOS  |= 0x10;                    /* Make channel an output compare  */
ECT_TC4    = ECT_TCNT + OSTickCnts;   /* Set TC4 to present time + OS_TICK_OC_CNTS */
ECT_TIE   |= 0x10;                    /* Enable OC4 interrupt */&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the above configuration the following lines of code work for HC9S12DP512 but not for MC9S12XEP100.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt; BSET  PTT, #$010
 BCLR  PTT, #$010&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, I would like to know why on HC9S12DP512 the above lines work even with Output Compare enabled and on MC9S12XEP100 it doesn't.&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 12:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1342760#M18180</guid>
      <dc:creator>danielflor</dc:creator>
      <dc:date>2021-09-20T12:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: Transferring code from HC9S12DP512 to MC9S12XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1342811#M18181</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;You are mixing two thing.&lt;/P&gt;
&lt;P&gt;A periheral ECT and a GPIO function.&lt;/P&gt;
&lt;P&gt;ECT as a peripheral can outomaticaly set/clear/togglo/do_nothing on output compare action if ECT peripheral is enabled at the pin. Moreover if the peripheral is enabled at he pin then it takes precedence over GPIO (the lowest alternative function of the pin)and also over all peripherals with lower prioritu connected to the pin. The priority of the alternative functions can be fond in the data sheet in the table (Table 1-10. Signal Properties Summary) which summarize functions for each pin. The priority of perihherals is from left to the right.&lt;/P&gt;
&lt;P&gt;Another thing is set or cler pin in the GPIO function. BSET/BCLR (PTT_PTT4 = 1; PTT_PTT4 = 0;). Of course if the ECT is enabled at the pin the GPIO function is not connected to the pin. You are writin to the buffer but the buffer is disconnected from them pin because ECT takes precedence.&lt;/P&gt;
&lt;P&gt;Now the question is what you want to do. Either toggle pin manually or generate output signal with automatic/manual action at the pin.&lt;/P&gt;
&lt;P&gt;I believe a set of examples can help you... &lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LAMA-s-S12XE-unofficial-examples/ta-p/1100774" target="_blank"&gt;https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LAMA-s-S12XE-unofficial-examples/ta-p/1100774&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The examples are compatible in principle because they are written for the same family devices.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 14:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1342811#M18181</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2021-09-20T14:45:26Z</dc:date>
    </item>
    <item>
      <title>Re: Transferring code from HC9S12DP512 to MC9S12XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1342819#M18182</link>
      <description>&lt;P&gt;I want to use Output Compare timer to generate tick for OS, but I have a device that is physically connected to pin PT4 and I would like to control it.&lt;BR /&gt;On the DP512, it is like this and when porting to the XEP100, the functionality that, in theory, had not changed, stopped working.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 15:13:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1342819#M18182</guid>
      <dc:creator>danielflor</dc:creator>
      <dc:date>2021-09-20T15:13:09Z</dc:date>
    </item>
    <item>
      <title>Re: Transferring code from HC9S12DP512 to MC9S12XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1343129#M18183</link>
      <description>&lt;P&gt;Hi Danielflor,&lt;/P&gt;
&lt;P&gt;minimum changes between ECT module on S12D and S12XE family, but one significant is still there.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;On S12D, the direct output compare action on pin is defined by TCTL1/TCTL2 configuration. I can imagine case when you set no action on pin and drive the pin by GPIO in interrupt routine. Please confirm, whether this is your case.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;On S12XE, the&amp;nbsp;TCTL1/TCTL2 configuration works similar, but OLx,OMx=0 will not automatically enable GPIO functionality on a pin. You have to additionally set the appropriate bit in the new OCPD register for disconnection port T pin from ECT driving. After that, you may use OC4 channel and GPIO function on PT4 simultaneously.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope it helps you.&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Radek&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 08:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1343129#M18183</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2021-09-21T08:55:18Z</dc:date>
    </item>
    <item>
      <title>Re: Transferring code from HC9S12DP512 to MC9S12XEP100</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1345225#M18189</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/40626"&gt;@RadekS&lt;/a&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;You got the key point.&lt;BR /&gt;I've set ECT_OCPD_OCPD4 = 0b1 and everything works like a charm now.&lt;BR /&gt;Thanks a lot&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 17:32:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Transferring-code-from-HC9S12DP512-to-MC9S12XEP100/m-p/1345225#M18189</guid>
      <dc:creator>danielflor</dc:creator>
      <dc:date>2021-09-23T17:32:30Z</dc:date>
    </item>
  </channel>
</rss>