<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I USE MOLLOC IN S12G in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-USE-MOLLOC-IN-S12G/m-p/1130958#M18070</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;us the tile， I use molloc function sucessfuly in S12G128 mcu。&lt;/P&gt;&lt;P&gt;and this way solve one bug that my code will stop at a &amp;nbsp;not certern position, because of the use of RAM.&lt;/P&gt;&lt;P&gt;Because , I just use a &amp;nbsp;buf[384] way for example, and so total RAM size is reduced.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But after use molloc way, this question is solved .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 May 2018 12:02:10 GMT</pubDate>
    <dc:creator>wojinandawei</dc:creator>
    <dc:date>2018-05-21T12:02:10Z</dc:date>
    <item>
      <title>I USE MOLLOC IN S12G</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-USE-MOLLOC-IN-S12G/m-p/1130958#M18070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;us the tile， I use molloc function sucessfuly in S12G128 mcu。&lt;/P&gt;&lt;P&gt;and this way solve one bug that my code will stop at a &amp;nbsp;not certern position, because of the use of RAM.&lt;/P&gt;&lt;P&gt;Because , I just use a &amp;nbsp;buf[384] way for example, and so total RAM size is reduced.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But after use molloc way, this question is solved .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 May 2018 12:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-USE-MOLLOC-IN-S12G/m-p/1130958#M18070</guid>
      <dc:creator>wojinandawei</dc:creator>
      <dc:date>2018-05-21T12:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: I USE MOLLOC IN S12G</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-USE-MOLLOC-IN-S12G/m-p/1327219#M18086</link>
      <description>&lt;P&gt;repeat&lt;/P&gt;</description>
      <pubDate>Sun, 22 Aug 2021 07:07:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-USE-MOLLOC-IN-S12G/m-p/1327219#M18086</guid>
      <dc:creator>aaronlee</dc:creator>
      <dc:date>2021-08-22T07:07:53Z</dc:date>
    </item>
    <item>
      <title>Re: I USE MOLLOC IN S12G</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-USE-MOLLOC-IN-S12G/m-p/1327220#M18087</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can refer&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Array-over-123-elements/m-p/672373" target="_blank" rel="noopener"&gt;Array over 123 elements&lt;/A&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;</description>
      <pubDate>Sun, 22 Aug 2021 07:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-USE-MOLLOC-IN-S12G/m-p/1327220#M18087</guid>
      <dc:creator>aaronlee</dc:creator>
      <dc:date>2021-08-22T07:05:23Z</dc:date>
    </item>
  </channel>
</rss>