<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 CAN Bus-off register in MSCAN</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-Bus-off-register-in-MSCAN/m-p/1289777#M17892</link>
    <description>&lt;P&gt;In&amp;nbsp;MSCAN Receiver Flag Register (CANRFLG), to monitor the Bus-off state which bits should we use in our software? In CANRFLG register, bits - RSTAT[1:0] or TSTAT[1:0] should we use to get the Bus-off status ?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jun 2021 08:45:55 GMT</pubDate>
    <dc:creator>pratibhasurabhi</dc:creator>
    <dc:date>2021-06-09T08:45:55Z</dc:date>
    <item>
      <title>CAN Bus-off register in MSCAN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-Bus-off-register-in-MSCAN/m-p/1289777#M17892</link>
      <description>&lt;P&gt;In&amp;nbsp;MSCAN Receiver Flag Register (CANRFLG), to monitor the Bus-off state which bits should we use in our software? In CANRFLG register, bits - RSTAT[1:0] or TSTAT[1:0] should we use to get the Bus-off status ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 08:45:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-Bus-off-register-in-MSCAN/m-p/1289777#M17892</guid>
      <dc:creator>pratibhasurabhi</dc:creator>
      <dc:date>2021-06-09T08:45:55Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Bus-off register in MSCAN</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-Bus-off-register-in-MSCAN/m-p/1289878#M17893</link>
      <description>&lt;P&gt;Hello Pratibhasurabhi,&lt;/P&gt;
&lt;P&gt;This MCU has implemented the MSCAN_V3 so you need to monitor TSTAT[1:0] bits the decode the Bus-off state. The information in RSTAT[1:0] is redundant as mentioned under Table 13-10 in RM. You can use the automatic recovery mode or use the BORM = 1 for recovery upon user request.&lt;/P&gt;
&lt;P&gt;I hope it helps you to solve your issue.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;Stano.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 11:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/CAN-Bus-off-register-in-MSCAN/m-p/1289878#M17893</guid>
      <dc:creator>StanoA</dc:creator>
      <dc:date>2021-06-09T11:22:39Z</dc:date>
    </item>
  </channel>
</rss>