<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: A problem about the algorithm of S-type acceleration and deceleration</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/A-problem-about-the-algorithm-of-S-type-acceleration-and/m-p/1285930#M17881</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;There is no such a function in the library yet, however, you can create one using basic blocks (e.g. two integrators in series with look-up tables of input jerk / acceleration limit, or, square root function directly).&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Matej&lt;/P&gt;</description>
    <pubDate>Wed, 02 Jun 2021 07:29:41 GMT</pubDate>
    <dc:creator>pachamatej</dc:creator>
    <dc:date>2021-06-02T07:29:41Z</dc:date>
    <item>
      <title>A problem about the algorithm of S-type acceleration and deceleration</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/A-problem-about-the-algorithm-of-S-type-acceleration-and/m-p/1284371#M17873</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Hello everyone, I am currently designing a BLDC driver based on position control。&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I use function the&amp;nbsp; libraries ，MC9S12ZVM_AMMCLIB_RTM_1_1_23_BIN.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Is there a function or reference design for T-type acceleration / deceleration or S-type acceleration / deceleration&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Thank you very much&lt;/P&gt;</description>
      <pubDate>Sat, 29 May 2021 09:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/A-problem-about-the-algorithm-of-S-type-acceleration-and/m-p/1284371#M17873</guid>
      <dc:creator>maxxu</dc:creator>
      <dc:date>2021-05-29T09:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: A problem about the algorithm of S-type acceleration and deceleration</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/A-problem-about-the-algorithm-of-S-type-acceleration-and/m-p/1285930#M17881</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;There is no such a function in the library yet, however, you can create one using basic blocks (e.g. two integrators in series with look-up tables of input jerk / acceleration limit, or, square root function directly).&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Matej&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 07:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/A-problem-about-the-algorithm-of-S-type-acceleration-and/m-p/1285930#M17881</guid>
      <dc:creator>pachamatej</dc:creator>
      <dc:date>2021-06-02T07:29:41Z</dc:date>
    </item>
  </channel>
</rss>