<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Re: ESD testing failure for MC9S12XET256MAG</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ESD-testing-failure-for-MC9S12XET256MAG/m-p/1268307#M17833</link>
    <description>&lt;P&gt;I have the same problem on the LS1043A chip, my work around is to program the hw watchdog to reset if the cores are frozen because of ESD.&lt;/P&gt;&lt;P&gt;Not the ideal solution but work for me.&lt;/P&gt;&lt;P&gt;Hope my comment helps you.&lt;/P&gt;</description>
    <pubDate>Mon, 26 Apr 2021 18:51:55 GMT</pubDate>
    <dc:creator>chithanhhoang</dc:creator>
    <dc:date>2021-04-26T18:51:55Z</dc:date>
    <item>
      <title>ESD testing failure for MC9S12XET256MAG</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ESD-testing-failure-for-MC9S12XET256MAG/m-p/1023570#M17045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we are using the controller MC9S12XET256MAG for our transmission ECU. While doing ESD test(Air discharge) near controller area, the controller is getting halt during&amp;nbsp;the exposure.It's recovering only after the hard reset of the device. Kindly suggest some solution to rectify the same.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2020 10:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ESD-testing-failure-for-MC9S12XET256MAG/m-p/1023570#M17045</guid>
      <dc:creator>kumara</dc:creator>
      <dc:date>2020-03-12T10:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: ESD testing failure for MC9S12XET256MAG</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ESD-testing-failure-for-MC9S12XET256MAG/m-p/1023571#M17046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;standard procedure.....&lt;/P&gt;&lt;P&gt;1) Could you please send a readable schematic of the MCU environment?&lt;/P&gt;&lt;P&gt;2) Also good to see whether PCB is OK especially all unused pins correctly (&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN3262.pdf" title="https://www.nxp.com/docs/en/application-note/AN3262.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3262.pdf&lt;/A&gt;&amp;nbsp;), no wire or plane under oscillator circuitry, correctly calculated load capacitances,.....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2020 06:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ESD-testing-failure-for-MC9S12XET256MAG/m-p/1023571#M17046</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2020-04-08T06:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: ESD testing failure for MC9S12XET256MAG</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ESD-testing-failure-for-MC9S12XET256MAG/m-p/1268307#M17833</link>
      <description>&lt;P&gt;I have the same problem on the LS1043A chip, my work around is to program the hw watchdog to reset if the cores are frozen because of ESD.&lt;/P&gt;&lt;P&gt;Not the ideal solution but work for me.&lt;/P&gt;&lt;P&gt;Hope my comment helps you.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 18:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/ESD-testing-failure-for-MC9S12XET256MAG/m-p/1268307#M17833</guid>
      <dc:creator>chithanhhoang</dc:creator>
      <dc:date>2021-04-26T18:51:55Z</dc:date>
    </item>
  </channel>
</rss>