<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 5V Power supply - Microcontroller  S912ZVCA19F0MKH in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/5V-Power-supply-Microcontroller-S912ZVCA19F0MKH/m-p/1246446#M17756</link>
    <description>&lt;P&gt;Hi, I would like to to power up the micro with a 5V power supply. I have seen from previous posts that to do so it is nesccesary to connect together all the bpower pins (VSUP, VDDC,VDDX,VDDA), but I was wondering if there is any official documentation on the issue, like an application note or similar.&lt;/P&gt;&lt;P&gt;Moreover, what I have to do with the ballast connections? Should I leave them floating?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;G. Pira&lt;/P&gt;</description>
    <pubDate>Tue, 16 Mar 2021 13:01:15 GMT</pubDate>
    <dc:creator>gpira</dc:creator>
    <dc:date>2021-03-16T13:01:15Z</dc:date>
    <item>
      <title>5V Power supply - Microcontroller  S912ZVCA19F0MKH</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/5V-Power-supply-Microcontroller-S912ZVCA19F0MKH/m-p/1246446#M17756</link>
      <description>&lt;P&gt;Hi, I would like to to power up the micro with a 5V power supply. I have seen from previous posts that to do so it is nesccesary to connect together all the bpower pins (VSUP, VDDC,VDDX,VDDA), but I was wondering if there is any official documentation on the issue, like an application note or similar.&lt;/P&gt;&lt;P&gt;Moreover, what I have to do with the ballast connections? Should I leave them floating?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;G. Pira&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 13:01:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/5V-Power-supply-Microcontroller-S912ZVCA19F0MKH/m-p/1246446#M17756</guid>
      <dc:creator>gpira</dc:creator>
      <dc:date>2021-03-16T13:01:15Z</dc:date>
    </item>
    <item>
      <title>Re: 5V Power supply - Microcontroller  S912ZVCA19F0MKH</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/5V-Power-supply-Microcontroller-S912ZVCA19F0MKH/m-p/1247144#M17764</link>
      <description>&lt;P&gt;Hi G. Pira,&lt;/P&gt;
&lt;P&gt;It is not officially supported and there is no such document.&lt;/P&gt;
&lt;P&gt;The VSUP pin must not be left unconnected.&lt;/P&gt;
&lt;P&gt;If you want to use an external 5V regulator, it must supply VSUP as well.&lt;/P&gt;
&lt;P&gt;The MagniV series is design for 12V systems, it has internal LDOs and, for example, the BATS module that monitors the VSUP power supply.&lt;/P&gt;
&lt;P&gt;Also, because the consumption of the CANPHY can be significant under certain conditions, the S12ZVC has a separate regulator for it.&lt;/P&gt;
&lt;P&gt;Please have a look at Appendix I S12CANPHY Electrical Specifications in the S12ZVC RM.&lt;/P&gt;
&lt;P&gt;If the ballast transistors are not used, the BCTL pins should be left unconnected.&lt;/P&gt;
&lt;P&gt;AN4867, Hardware Design Guidelines for S12ZVC, Chapter 11 Unused pins.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-magniv-mixed-signal-mcus/s12zvc-mixed-signal-mcu-for-automotive-industrial-can-applications:S12ZVC?tab=Documentation_Tab" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-magniv-mixed-signal-mcus/s12zvc-mixed-signal-mcu-for-automotive-industrial-can-applications:S12ZVC?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 10:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/5V-Power-supply-Microcontroller-S912ZVCA19F0MKH/m-p/1247144#M17764</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-03-17T10:21:33Z</dc:date>
    </item>
  </channel>
</rss>