<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MM9Z1638D1 cranking mode in S12 / MagniV Microcontrollers</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1638D1-cranking-mode/m-p/1230973#M17724</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I strongly recommend to NOT use the cranking mode feature. &lt;STRONG&gt;It would be better to analyze which issue you are trying to solve and to find an alternative approach!&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;I'm not aware of any customer using this feature and I have not used it myself. I expect to have many corner cases of external conditions (e.g. dV/dt of VSUP) and SW handling the process of entering low power mode and exiting it again. So I will not be of much help here.&lt;/P&gt;
&lt;P&gt;The UVI is related to the analog die VSUP monitoring. It will typically occur at 5.2V (see Datasheet Table 12. Static electrical characteristics - power supply) and will issue an D2D interrupt if enabled see 6.7.2.4.1Undervoltage Interrupt (UVI)).&lt;/P&gt;
&lt;P&gt;The RAM is initialize during the uC Reset to all zeros. This is required to avoid any unintentional ECC errors (see&amp;nbsp; 6.8.3.4 Memory initialization)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Rgds&lt;/P&gt;
&lt;P&gt;W.&lt;/P&gt;</description>
    <pubDate>Mon, 15 Feb 2021 12:26:06 GMT</pubDate>
    <dc:creator>Q_man</dc:creator>
    <dc:date>2021-02-15T12:26:06Z</dc:date>
    <item>
      <title>MM9Z1638D1 cranking mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1638D1-cranking-mode/m-p/1230655#M17723</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am thinking about using "cranking mode" for preserving contents of RAM in case of under voltage on MM9Z1638D1. Per the reference manual, I can enter cranking mode by writing 0x0303 to PCR_CTL. The flow chart attached here mentions entering cranking mode on UVI or undervoltage interrupt. But I couldn't find vector address for UVI in the reference manual. My initial thought was to write an UVI service routine. Can you help me with this?&lt;/P&gt;&lt;P&gt;Secondly, how to get out of cranking mode?&lt;/P&gt;&lt;P&gt;Finally, once the power on reset threshold is reached the contents of RAM become invalid?&lt;/P&gt;</description>
      <pubDate>Sat, 13 Feb 2021 00:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1638D1-cranking-mode/m-p/1230655#M17723</guid>
      <dc:creator>mihir_rajput</dc:creator>
      <dc:date>2021-02-13T00:55:31Z</dc:date>
    </item>
    <item>
      <title>Re: MM9Z1638D1 cranking mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1638D1-cranking-mode/m-p/1230973#M17724</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I strongly recommend to NOT use the cranking mode feature. &lt;STRONG&gt;It would be better to analyze which issue you are trying to solve and to find an alternative approach!&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;I'm not aware of any customer using this feature and I have not used it myself. I expect to have many corner cases of external conditions (e.g. dV/dt of VSUP) and SW handling the process of entering low power mode and exiting it again. So I will not be of much help here.&lt;/P&gt;
&lt;P&gt;The UVI is related to the analog die VSUP monitoring. It will typically occur at 5.2V (see Datasheet Table 12. Static electrical characteristics - power supply) and will issue an D2D interrupt if enabled see 6.7.2.4.1Undervoltage Interrupt (UVI)).&lt;/P&gt;
&lt;P&gt;The RAM is initialize during the uC Reset to all zeros. This is required to avoid any unintentional ECC errors (see&amp;nbsp; 6.8.3.4 Memory initialization)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Rgds&lt;/P&gt;
&lt;P&gt;W.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Feb 2021 12:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1638D1-cranking-mode/m-p/1230973#M17724</guid>
      <dc:creator>Q_man</dc:creator>
      <dc:date>2021-02-15T12:26:06Z</dc:date>
    </item>
    <item>
      <title>Re: MM9Z1638D1 cranking mode</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1638D1-cranking-mode/m-p/1230974#M17725</link>
      <description>&lt;P&gt;Leaving "cranking mode" will be through wakeup from STOP condition! E.g. after predefined time.&lt;/P&gt;
&lt;P&gt;W.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Feb 2021 12:29:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MM9Z1638D1-cranking-mode/m-p/1230974#M17725</guid>
      <dc:creator>Q_man</dc:creator>
      <dc:date>2021-02-15T12:29:23Z</dc:date>
    </item>
  </channel>
</rss>