<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックRe: S12Z fails to boot</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1226365#M17718</link>
    <description>&lt;P&gt;Hello Lu,&lt;/P&gt;
&lt;P&gt;It is hard to say.&lt;/P&gt;
&lt;P&gt;Even the capacitor can be burnt - there can be a short to the ground.&lt;/P&gt;
&lt;P&gt;Can you share the whole schematic?&lt;/P&gt;
&lt;P&gt;You can create a ticket if you do not want to share it here.&lt;/P&gt;
&lt;P&gt;Is the TEST pin tied to the ground?&lt;/P&gt;
&lt;P&gt;Is the MCU heating or is the power consumption of the failed part higher than usual?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Feb 2021 11:07:20 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2021-02-04T11:07:20Z</dc:date>
    <item>
      <title>S12Z fails to boot</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1219684#M17695</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; My group met a problem that some of our controllers using S12ZVC failed to boot. The defective rate is about 0.1%。&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; The phenomenons list as below:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; 1、turn on the battery, the LDO chip normally sends out VCC 15V while the S12ZVC doesn't boot. VDDX pin on BDM interface is 5V, which is generated from the external PNP controlled by the&amp;nbsp;BCTL pin. Reset pin on BDM is 0.2V.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;2、Then, plug in the universal multilink debugger, the S12ZVC boot for a uncertain period of time, sometimes several seconds and sometimes several minutes.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;3、Connecting a 4.7k resistor to pull up the reset pin externally doesn't solve the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Since the status is not stable, it is not able to check the registers in debugging mode on the IDE.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Any suggestions to find out what has happened to the chip?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Thank you!&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jan 2021 15:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1219684#M17695</guid>
      <dc:creator>thulzh</dc:creator>
      <dc:date>2021-01-22T15:08:57Z</dc:date>
    </item>
    <item>
      <title>Re: S12Z fails to boot</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1220414#M17698</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;You can refer to the Power On Reset Sequence in the S12ZVM RM, it is the same for S12ZVC.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1611567517194.png" style="width: 619px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135675i4DFA924683E0D718/image-dimensions/619x467?v=v2" width="619" height="467" role="button" title="danielmartynek_0-1611567517194.png" alt="danielmartynek_0-1611567517194.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1611567517194.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-magniv-mixed-signal-mcus/s12zvm-mixed-signal-mcu-for-automotive-industrial-motor-control-applications:S12ZVM?tab=Documentation_Tab" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-magniv-mixed-signal-mcus/s12zvm-mixed-signal-mcu-for-automotive-industrial-motor-control-applications:S12ZVM?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Can you scope VDD, VDDF, VDDA, VDDX along with the reset pin?&lt;/P&gt;
&lt;P&gt;Is the reset pin disconnected from any other circuit on the board?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 09:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1220414#M17698</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-01-25T09:44:13Z</dc:date>
    </item>
    <item>
      <title>Re: S12Z fails to boot</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1223558#M17709</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your suggestions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;The S12Z has been covered by thermal compounds which is not able to be removed. Thus, I am not able to scope the VDDA VSUP pin. Fortunately, VDDX pin, connected to the external PNP, can be scope along with the reset pin. In the following graphs, the yellow signal&amp;nbsp;is 'reset' and the blue signal is 'VDDX'. The normally working one is list first followed by the faulted one.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fig 1" style="width: 800px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136136i4B3F3B29CF91F775/image-size/large?v=v2&amp;amp;px=999" role="button" title="pic_530_3.gif" alt="fig 1" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fig 1&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fig 2" style="width: 800px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136137i2EB8A90652435E08/image-size/large?v=v2&amp;amp;px=999" role="button" title="pic_530_2.gif" alt="fig 2" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fig 2&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It shows that a sharp raising edge was missing in the faulted case although the tendency was similiar . There is a 10pF capacitor on the reset pin on both controller.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lu&lt;/P&gt;</description>
      <pubDate>Sat, 30 Jan 2021 17:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1223558#M17709</guid>
      <dc:creator>thulzh</dc:creator>
      <dc:date>2021-01-30T17:03:01Z</dc:date>
    </item>
    <item>
      <title>Re: S12Z fails to boot</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1224059#M17710</link>
      <description>&lt;P&gt;Hi Lu,&lt;/P&gt;
&lt;P&gt;In fig 2, we can see that the MCU releases the reset pin when VDDX reaches the LVR threshold voltage.&lt;/P&gt;
&lt;P&gt;S12ZVC RM rev.2.1, Table E-1.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1612179457482.png" style="width: 694px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136214i37D08EC33887A58C/image-dimensions/694x59?v=v2" width="694" height="59" role="button" title="danielmartynek_0-1612179457482.png" alt="danielmartynek_0-1612179457482.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1612179457482.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If it is not driven externally, the reset pin is then pulled to VDDX by the internal pull-up resistor.&lt;/P&gt;
&lt;P&gt;Table A-8.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_1-1612179622194.png" style="width: 642px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136215iE81E53BE32D8FEFB/image-dimensions/642x106?v=v2" width="642" height="106" role="button" title="danielmartynek_1-1612179622194.png" alt="danielmartynek_1-1612179622194.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_1-1612179622194.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;What is connected to the reset pin besides the capacitor that you mentioned?&lt;/P&gt;
&lt;P&gt;Can you disconnect everything including the debugger?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 11:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1224059#M17710</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-02-01T11:44:40Z</dc:date>
    </item>
    <item>
      <title>Re: S12Z fails to boot</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1224187#M17711</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;The figures I have posted was captured without debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In theory, nothing is connected to the reset pin except for the capacitor mentioned.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fig 1" style="width: 497px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136222i6A88E3B26624575A/image-size/large?v=v2&amp;amp;px=999" role="button" title="tmp.jpg" alt="fig 1" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fig 1&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;So,&amp;nbsp;&amp;nbsp;whether can it&amp;nbsp;be said that it may be a problem related to the manufacturing process, such as bad soldering,&amp;nbsp;external component damage, rather than a chip problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Lu&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 17:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1224187#M17711</guid>
      <dc:creator>thulzh</dc:creator>
      <dc:date>2021-02-01T17:11:36Z</dc:date>
    </item>
    <item>
      <title>Re: S12Z fails to boot</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1226365#M17718</link>
      <description>&lt;P&gt;Hello Lu,&lt;/P&gt;
&lt;P&gt;It is hard to say.&lt;/P&gt;
&lt;P&gt;Even the capacitor can be burnt - there can be a short to the ground.&lt;/P&gt;
&lt;P&gt;Can you share the whole schematic?&lt;/P&gt;
&lt;P&gt;You can create a ticket if you do not want to share it here.&lt;/P&gt;
&lt;P&gt;Is the TEST pin tied to the ground?&lt;/P&gt;
&lt;P&gt;Is the MCU heating or is the power consumption of the failed part higher than usual?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 11:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1226365#M17718</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-02-04T11:07:20Z</dc:date>
    </item>
    <item>
      <title>Re: S12Z fails to boot</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1584190#M19035</link>
      <description>&lt;P&gt;This may help, but I think u need a pullup on the BKGD pin that also functions as the MODC or mode select pin which determines its in Normal Single-Chip Mode or Special Single-Chip Mode.&lt;/P&gt;&lt;P&gt;Just found this out over here, may or may not be the solution but worked for me. &lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/New-DEVKIT-S12ZCV-Fails-to-boot/m-p/1583459#M19033" target="_blank"&gt;https://community.nxp.com/t5/S12-MagniV-Microcontrollers/New-DEVKIT-S12ZCV-Fails-to-boot/m-p/1583459#M19033&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 21:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-fails-to-boot/m-p/1584190#M19035</guid>
      <dc:creator>nateimig</dc:creator>
      <dc:date>2023-01-17T21:31:45Z</dc:date>
    </item>
  </channel>
</rss>