<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 MFR4310 communication issue</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MFR4310-communication-issue/m-p/1222968#M17706</link>
    <description>&lt;P&gt;Dear:&lt;/P&gt;&lt;P class="tgt"&gt;&lt;SPAN class="tgt highlight"&gt;We have a project that uses MFR4310 and TJA1082 to communicate with&amp;nbsp; FlexRay nodes.&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt;When sending data, the receiving node will detect the phenomenon that a frame of data is sent repeatedly occasionally, and the repeated data frames are not fixed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="tgt"&gt;&lt;SPAN class="tgt"&gt;Example of data transmission mode: in one time interval, two frames of data with ID 1 and 2 are first sent, then the ID are added 1, and the data with ID 3 and 4 are sent, and repeated successively.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="tgt"&gt;&lt;SPAN class="tgt"&gt;So Data frames with Frame ID 1,2,3,4,5,6,7,8 are sent on the FlexRay bus.&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt;However, the receiving data will have Frame ID of 1,2,3,3,5,6,7,8 or 1,2,3,4,5,5,7,8.&amp;nbsp;&lt;SPAN&gt;A frame is repeated and a frame is missed&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="tgt"&gt;&lt;SPAN class="tgt"&gt;At present, only one board appears this problem, do not understand the cause of this issue.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt;Please help to analyze it.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 29 Jan 2021 02:27:33 GMT</pubDate>
    <dc:creator>Makabaka</dc:creator>
    <dc:date>2021-01-29T02:27:33Z</dc:date>
    <item>
      <title>MFR4310 communication issue</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MFR4310-communication-issue/m-p/1222968#M17706</link>
      <description>&lt;P&gt;Dear:&lt;/P&gt;&lt;P class="tgt"&gt;&lt;SPAN class="tgt highlight"&gt;We have a project that uses MFR4310 and TJA1082 to communicate with&amp;nbsp; FlexRay nodes.&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt;When sending data, the receiving node will detect the phenomenon that a frame of data is sent repeatedly occasionally, and the repeated data frames are not fixed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="tgt"&gt;&lt;SPAN class="tgt"&gt;Example of data transmission mode: in one time interval, two frames of data with ID 1 and 2 are first sent, then the ID are added 1, and the data with ID 3 and 4 are sent, and repeated successively.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="tgt"&gt;&lt;SPAN class="tgt"&gt;So Data frames with Frame ID 1,2,3,4,5,6,7,8 are sent on the FlexRay bus.&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt;However, the receiving data will have Frame ID of 1,2,3,3,5,6,7,8 or 1,2,3,4,5,5,7,8.&amp;nbsp;&lt;SPAN&gt;A frame is repeated and a frame is missed&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="tgt"&gt;&lt;SPAN class="tgt"&gt;At present, only one board appears this problem, do not understand the cause of this issue.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt;Please help to analyze it.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jan 2021 02:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MFR4310-communication-issue/m-p/1222968#M17706</guid>
      <dc:creator>Makabaka</dc:creator>
      <dc:date>2021-01-29T02:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: MFR4310 communication issue</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MFR4310-communication-issue/m-p/1227201#M17721</link>
      <description>&lt;P&gt;The issue is under a discussion here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/MFR4310-commnication-issue/m-p/1226267#M10412" target="_blank"&gt;https://community.nxp.com/t5/Other-NXP-Products/MFR4310-commnication-issue/m-p/1226267#M10412&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Feb 2021 15:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/MFR4310-communication-issue/m-p/1227201#M17721</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-02-05T15:01:58Z</dc:date>
    </item>
  </channel>
</rss>