<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollers中的主题 Read Content of P_Flash From BootLoader</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Read-Content-of-P-Flash-From-BootLoader/m-p/1176246#M17564</link>
    <description>&lt;P&gt;Hi, I'm working on a bootloader program based on AN4258 application note for MC9S12G128. I'm downloading program from CAN and saving the content on P-Flash addresses mentioned in s19 file. After writing is finished, I want to check that if data written correctly. CRC32 is used for this purpose. But when I want to read the content of P-Flash addresses using pointers, it returns me 0xFF or 0x00. I have multilink &amp;amp; can see the amount of Flash in Hi-wave is correct. Any guide to read content of P-Flash correctly. It that cause can it be used as EEPROM for writing data?&lt;/P&gt;&lt;P&gt;Thanks for your responses.&lt;/P&gt;</description>
    <pubDate>Sun, 01 Nov 2020 15:02:58 GMT</pubDate>
    <dc:creator>margieenovak</dc:creator>
    <dc:date>2020-11-01T15:02:58Z</dc:date>
    <item>
      <title>Read Content of P_Flash From BootLoader</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Read-Content-of-P-Flash-From-BootLoader/m-p/1176246#M17564</link>
      <description>&lt;P&gt;Hi, I'm working on a bootloader program based on AN4258 application note for MC9S12G128. I'm downloading program from CAN and saving the content on P-Flash addresses mentioned in s19 file. After writing is finished, I want to check that if data written correctly. CRC32 is used for this purpose. But when I want to read the content of P-Flash addresses using pointers, it returns me 0xFF or 0x00. I have multilink &amp;amp; can see the amount of Flash in Hi-wave is correct. Any guide to read content of P-Flash correctly. It that cause can it be used as EEPROM for writing data?&lt;/P&gt;&lt;P&gt;Thanks for your responses.&lt;/P&gt;</description>
      <pubDate>Sun, 01 Nov 2020 15:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Read-Content-of-P-Flash-From-BootLoader/m-p/1176246#M17564</guid>
      <dc:creator>margieenovak</dc:creator>
      <dc:date>2020-11-01T15:02:58Z</dc:date>
    </item>
  </channel>
</rss>