<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollersのトピックsome Question about the function &amp;quot;adc&amp;quot;  when i use s12zvml128 control pmsm foc (MC9S12ZVML128_PMSM_)</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/some-Question-about-the-function-quot-adc-quot-when-i-use/m-p/1171506#M17547</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I use the single resistance sampling mode without a reference voltage of 2.5V. At present, I can only sample the current in one direction. Can I use the current demo simply to modify it? What is the efficiency?&lt;/P&gt;&lt;P&gt;Is there any problem. In addition, when the single resistance bus sampling will appear negative current?&lt;/P&gt;</description>
    <pubDate>Thu, 22 Oct 2020 03:31:09 GMT</pubDate>
    <dc:creator>Clarkhe</dc:creator>
    <dc:date>2020-10-22T03:31:09Z</dc:date>
    <item>
      <title>some Question about the function "adc"  when i use s12zvml128 control pmsm foc (MC9S12ZVML128_PMSM_)</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/some-Question-about-the-function-quot-adc-quot-when-i-use/m-p/1171506#M17547</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I use the single resistance sampling mode without a reference voltage of 2.5V. At present, I can only sample the current in one direction. Can I use the current demo simply to modify it? What is the efficiency?&lt;/P&gt;&lt;P&gt;Is there any problem. In addition, when the single resistance bus sampling will appear negative current?&lt;/P&gt;</description>
      <pubDate>Thu, 22 Oct 2020 03:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/some-Question-about-the-function-quot-adc-quot-when-i-use/m-p/1171506#M17547</guid>
      <dc:creator>Clarkhe</dc:creator>
      <dc:date>2020-10-22T03:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: some Question about the function "adc"  when i use s12zvml128 control pmsm foc (MC9S12</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/some-Question-about-the-function-quot-adc-quot-when-i-use/m-p/1172482#M17548</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I'm not sure if I understand.&lt;/P&gt;
&lt;P&gt;Can you please elaborate?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Oct 2020 13:22:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/some-Question-about-the-function-quot-adc-quot-when-i-use/m-p/1172482#M17548</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-10-23T13:22:28Z</dc:date>
    </item>
    <item>
      <title>Re: some Question about the function "adc"  when i use s12zvml128 control pmsm foc (MC9S12</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/some-Question-about-the-function-quot-adc-quot-when-i-use/m-p/1173194#M17552</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I'm just assuming, so if I'm not correct, please clarify.&lt;/P&gt;
&lt;P&gt;In case you are using our devkits&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solutions/3-phase-sensorless-pmsm-development-kit-with-s12-magniv-mc9s12zvml128-mcu:MTRCKTSPNZVM128" target="_blank"&gt;https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solutions/3-phase-sensorless-pmsm-development-kit-with-s12-magniv-mc9s12zvml128-mcu:MTRCKTSPNZVM128&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solutions/s12zvm-mini-board-and-mini-kit-evaluation-platforms:S12ZVML-MINIXXX" target="_blank"&gt;https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solutions/s12zvm-mini-board-and-mini-kit-evaluation-platforms:S12ZVML-MINIXXX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solutions/s12zvm-evaluation-board-for-high-current-bldc-and-pmsm-motor-control:MCSXSR1CS12ZVM" target="_blank"&gt;https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/magniv-and-s12-solutions/s12zvm-evaluation-board-for-high-current-bldc-and-pmsm-motor-control:MCSXSR1CS12ZVM&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;All three boards are capable of using DC-link shunt resistor to control a 3-ph motor, but the last two can do only this technique (aka "single-shunt" only).&lt;/P&gt;
&lt;P&gt;If you are using the&amp;nbsp;MTRCKTSPNZVM128 or&amp;nbsp;MTRCKTSBNZVM128 (physically, it is the same devkit), then I would recommend to verify the jumper settings first according to the Quick start guide and the dedicated application note - there is a different configuration for dual-shunt and for single-shunt.&lt;/P&gt;
&lt;P&gt;By the way, in all the cases, the reference voltage is 2.5V and thanks to that, the ADC can see positive and negative currents.&lt;/P&gt;
&lt;P&gt;If you see any difference from what you want to achieve and from the description above, please let us know.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;
&lt;P&gt;Matej&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 14:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/some-Question-about-the-function-quot-adc-quot-when-i-use/m-p/1173194#M17552</guid>
      <dc:creator>pachamatej</dc:creator>
      <dc:date>2020-10-26T14:41:21Z</dc:date>
    </item>
    <item>
      <title>Re: some Question about the function "adc"  when i use s12zvml128 control pmsm foc (MC9S12</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/some-Question-about-the-function-quot-adc-quot-when-i-use/m-p/1173646#M17556</link>
      <description>&lt;P&gt;OK,thankyou&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 07:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/some-Question-about-the-function-quot-adc-quot-when-i-use/m-p/1173646#M17556</guid>
      <dc:creator>Clarkhe</dc:creator>
      <dc:date>2020-10-27T07:49:48Z</dc:date>
    </item>
  </channel>
</rss>