<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV Microcontrollersのトピック/XCLKS Is direct grounding OK?</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XCLKS-Is-direct-grounding-OK/m-p/1166551#M17525</link>
    <description>&lt;P&gt;&lt;SPAN&gt;My CPU is mc9s12xe series，The external crystal oscillator is used。&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Oct 2020 07:20:33 GMT</pubDate>
    <dc:creator>nxpxhy13</dc:creator>
    <dc:date>2020-10-13T07:20:33Z</dc:date>
    <item>
      <title>/XCLKS Is direct grounding OK?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XCLKS-Is-direct-grounding-OK/m-p/1166551#M17525</link>
      <description>&lt;P&gt;&lt;SPAN&gt;My CPU is mc9s12xe series，The external crystal oscillator is used。&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 07:20:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XCLKS-Is-direct-grounding-OK/m-p/1166551#M17525</guid>
      <dc:creator>nxpxhy13</dc:creator>
      <dc:date>2020-10-13T07:20:33Z</dc:date>
    </item>
    <item>
      <title>Re: /XCLKS Is direct grounding OK?</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XCLKS-Is-direct-grounding-OK/m-p/1167323#M17533</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;To configure the the oscillator for Full Swing Pierce or for an external clock source, the pin must read LOW during rising edge of the reset pin signal.&lt;/P&gt;
&lt;P&gt;It can be either driven or pulled externally.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please note that the the pin has an internal weak pullup enabled by default out of reset.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1602665365520.png" style="width: 604px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/127404i6414A80997CEA1D7/image-dimensions/604x71?v=v2" width="604" height="71" role="button" title="danielmartynek_0-1602665365520.png" alt="danielmartynek_0-1602665365520.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So, if an external pull-down is used, it must be stronger than that to ensure the logic value and compensate for noise.&lt;/P&gt;
&lt;P&gt;If the pin is connected to the ground directly, make sure the SW does not reconfigure the pin to GPIO Output and does not drive it HIGH.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Reference schematics for S12(X) devices:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reference-schematics-for-S12-X-devices/ta-p/1117869" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reference-schematics-for-S12-X-devices/ta-p/1117869&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_1-1602665602931.png" style="width: 607px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/127405iB4E242CF81E58977/image-dimensions/607x317?v=v2" width="607" height="317" role="button" title="danielmartynek_1-1602665602931.png" alt="danielmartynek_1-1602665602931.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 08:56:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/XCLKS-Is-direct-grounding-OK/m-p/1167323#M17533</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-10-14T08:56:18Z</dc:date>
    </item>
  </channel>
</rss>