<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S12 / MagniV MicrocontrollersのトピックS9S12XHY128F0VLM IO Problem</title>
    <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S9S12XHY128F0VLM-IO-Problem/m-p/1162306#M17505</link>
    <description>&lt;P&gt;S9S12XHY128F0VLMR is used for instrument products, and low pressure judgment needs to be made through pin3 port of the MCU PT0 pin docking plug-in.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When the instrument is in low-voltage working mode, pin3 port is not connected to low level, and PT0 pin is judged to be low level, which triggers the related alarm function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;After testing, if pin PT0 is below 3.5V, it will be judged as low level, and the register value is set to 0 by 1, making an error (at present, the software register reads the code: _pTI@ (0x0000 + 0x00000241UL);)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How to change the software so that the PT0 pin is judged as high level above 2V voltage?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 02 Oct 2020 14:56:53 GMT</pubDate>
    <dc:creator>jack_huang1</dc:creator>
    <dc:date>2020-10-02T14:56:53Z</dc:date>
    <item>
      <title>S9S12XHY128F0VLM IO Problem</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S9S12XHY128F0VLM-IO-Problem/m-p/1162306#M17505</link>
      <description>&lt;P&gt;S9S12XHY128F0VLMR is used for instrument products, and low pressure judgment needs to be made through pin3 port of the MCU PT0 pin docking plug-in.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When the instrument is in low-voltage working mode, pin3 port is not connected to low level, and PT0 pin is judged to be low level, which triggers the related alarm function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;After testing, if pin PT0 is below 3.5V, it will be judged as low level, and the register value is set to 0 by 1, making an error (at present, the software register reads the code: _pTI@ (0x0000 + 0x00000241UL);)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How to change the software so that the PT0 pin is judged as high level above 2V voltage?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Oct 2020 14:56:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S9S12XHY128F0VLM-IO-Problem/m-p/1162306#M17505</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2020-10-02T14:56:53Z</dc:date>
    </item>
    <item>
      <title>Re: S9S12XHY128F0VLM IO Problem</title>
      <link>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S9S12XHY128F0VLM-IO-Problem/m-p/1162933#M17507</link>
      <description>&lt;P&gt;Hello Jack,&lt;/P&gt;
&lt;P&gt;This cannot be changed by the software.&lt;BR /&gt;The datasheet guarantees that the port reads LOW when Vi is &amp;lt; VDD35 * 0.35 and HIGH when Vi is &amp;gt; VDD35 * 0.65.&lt;BR /&gt;Vi in the range of (VDD35 * 0.35; VDD35 * 0.65) can be read either as HIGH or LOW with hysteresis of 250mV.&lt;/P&gt;
&lt;P&gt;S12XHY datasheet:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1601903159933.png" style="width: 608px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126765i792CDCB524E0BB85/image-dimensions/608x184?v=v2" width="608" height="184" role="button" title="danielmartynek_0-1601903159933.png" alt="danielmartynek_0-1601903159933.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1601903159933.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;AN2434 Input/Output (I/O) Pin Drivers on HCS12 Family MCUs&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2434.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN2434.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2020 13:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S9S12XHY128F0VLM-IO-Problem/m-p/1162933#M17507</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-10-05T13:09:37Z</dc:date>
    </item>
  </channel>
</rss>